STM32F746IGT , 7 inch display With TouchGFX issues?
Hai
i have a STM32F746IGT Development board and (Waveshare) 7inch display(800x480).
Using tools are following bellow;
STM32CubeIDE 1.6.1
TouchGFX 4.16.0
STM32CubeMX 6.2.1
- while run the code it's go to Hard Fault ();
- after doing some change in LTDC start Frame Buffer address and some were it work fine. if there any changes in screen using TouchGFX tool display is also update.(Note: while display working time it's not enter the While() loop function)
- Once switch OFF and ON the controller come back to fist position.
I change Stack Size is also it not work.
Searching in internet related this issues but not find anything.
i am facing this issues for long time.
any one please share solution for this problems.
Please find the attachment of Program file for reference.
where i am doing make mistakes....? i need change hardware or code........?
Thanks you
by
M.Govind