Skip to main content
BJAUM
Visitor II
Sep 26, 2018 10:56 AM UTC
Question

STM32F746G-DISCO Touchscreen gestureId issues

Hi,

I'm working on a project which needs to ​get the gesture of the user on the touchscreen.

Apparently the "BSP_TS_GetState(TS_StateTypeDef *TS_State)" function fills a structure of TS_StateTypeDef type.

typedef struct
{
 uint8_t touchDetected;
 uint16_t touchX[TS_MAX_NB_TOUCH];
 uint16_t touchY[TS_MAX_NB_TOUCH];
 
#if (TS_MULTI_TOUCH_SUPPORTED == 1)
 uint8_t touchWeight[TS_MAX_NB_TOUCH];
 uint8_t touchEventId[TS_MAX_NB_TOUCH];
 uint8_t touchArea[TS_MAX_NB_TOUCH];
 uint32_t gestureId;
#endif
 
} TS_StateTypeDef;

The ​TS_StateTypeDef contains the gestureId variable which takes the value of type @ref TS_GestureIdTypeDef. (GEST_ID_MOVE_UP, GEST_ID_MOVE_DOWN...)

typedef enum
{
 GEST_ID_NO_GESTURE = 0x00, /*!< Gesture not defined / recognized */
 GEST_ID_MOVE_UP = 0x01, /*!< Gesture Move Up */
 GEST_ID_MOVE_RIGHT = 0x02, /*!< Gesture Move Right */
 GEST_ID_MOVE_DOWN = 0x03, /*!< Gesture Move Down */
 GEST_ID_MOVE_LEFT = 0x04, /*!< Gesture Move Left */
 GEST_ID_ZOOM_IN = 0x05, /*!< Gesture Zoom In */
 GEST_ID_ZOOM_OUT = 0x06, /*!< Gesture Zoom Out */
 GEST_ID_NB_MAX = 0x07 /*!< max number of gesture id */
 
} TS_GestureIdTypeDef;

So in my program i wrote :

//The full code is way more complicated, this part is just the problematic part
TS_StateTypeDef TS_Status; //My structure which will contain all the Touchscreen Datas
char buffer[50];//Text buffer
 
int main(void)
{
 //Fill the TS_Status structure with the Touchscreen datas 
 BSP_TS_GetState(&TS_Status);
 
 //Display on the LCD the TS_Status.gestureId Variable
 sprintf(buffer, "%d", TS_Status.gestureId);
 BSP_LCD_DisplayStringAt(0, LINE(0), &buffer, LEFT_MODE);
}

The problem is that BSP_TS_GetState(&TS_Status) always returns TS_Status.gestureId at 0, even if i move my finger up, down, left...

I already tried with the BSP_TS_Get_GestureId(&TS_State) function, same problem...

Thank you for your help,

Mathieu.

This topic has been closed for replies.

4 replies

Amel NASRI
ST Technical Moderator
Sep 26, 2018 5:05 PM UTC

Hi @BJAUM​ ,

Is only the gestureId which is wrong?

What do you get if you want to display touchX and touchY for example?

For the gestureId, you need to call ts_gesture_id_string_tab like what it is already done in STM32Cube_FW_F7_V1.12.0\Projects\STM32F769I-Discovery\Examples\BSP\Src\touchscreen.c:

 /* Get updated gesture Id in global variable 'TS_State' */
 ts_status = BSP_TS_Get_GestureId(&TS_State);
 
 sprintf((char*)lcd_string, "Gesture Id = %s", ts_gesture_id_string_tab[TS_State.gestureId]);
 BSP_LCD_SetTextColor(LCD_COLOR_WHITE);
 BSP_LCD_DisplayStringAt(0, BSP_LCD_GetYSize() - 15, lcd_string, CENTER_MODE);

Please try this way and let me know if this works for you.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Amel NASRI
ST Technical Moderator
Sep 26, 2018 5:14 PM UTC

I would like to add that ts_gesture_id_string_tab is declared in STM32Cube_FW_F7_V1.12.0\Drivers\BSP\STM32F769I-Discovery\stm32f769i_discovery_ts.c as following:

/* Table for touchscreen gesture Id information display on LCD : table indexed on enum @ref TS_GestureIdTypeDef information */
char * ts_gesture_id_string_tab[GEST_ID_NB_MAX] = { "None",
 "Move Up",
 "Move Right",
 "Move Down",
 "Move Left",
 "Zoom In",
 "Zoom Out"
 };
 

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
john doe
Senior III
Sep 26, 2018 8:27 PM UTC

the firmware of the touch screen controller that st used, does not have gestures enabled

MWang.2
Visitor II
Mar 2, 2020 7:21 AM UTC

Hi,BJAUM:

Have you fixed this issue, I'm confused about the issue too.