Skip to main content
Karan 123
Senior
December 23, 2019
Question

STM32F746G-DISCO : TouchGFX Run Target Fail

Hi

I am using TouchGFX  4.12.3 with STM32F746G-DISCO Board.

I have already installed STLink and STCubeProgrammer.

I am able to GUI run on simulator but not on target .

Please check below logs.

--

Thanks

Gurpreet Singh

This topic has been closed for replies.

3 replies

Karan 123
Karan 123Author
Senior
December 23, 2019
Run Target
 
 Generate
 
 Done
 
 Generate Assets
 
 make -f simulator/gcc/Makefile assets -j10
 
 Converting images
 
 Done
 
 Post Generate
 
 touchgfx update_project --project-file=../EWARM/MyApplication_3.ewp --gui-group-name=Application/User/TouchGFX/gui --generated-group-name=Application/User/TouchGFX/generated && touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
 
 Done
 
 Compile
 
 make -f ../gcc/Makefile -j8
 
 Converting images
 
 Compiling TouchGFX/gui/src/screen1_screen/Screen1Presenter.cpp
 
 Compiling TouchGFX/generated/fonts/src/Font_verdana_20_4bpp_0.cpp
 
 Compiling TouchGFX/gui/src/common/FrontendApplication.cpp
 
 Compiling TouchGFX/gui/src/screen1_screen/Screen1View.cpp
 
 Compiling TouchGFX/generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
 
 Compiling TouchGFX/generated/fonts/src/Font_verdana_40_4bpp_0.cpp
 
 Compiling TouchGFX/gui/src/model/Model.cpp
 
 Compiling TouchGFX/generated/gui_generated/src/common/FrontendApplicationBase.cpp
 
 Compiling TouchGFX/generated/fonts/src/GeneratedFont.cpp
 
 Compiling TouchGFX/generated/fonts/src/Kerning_verdana_40_4bpp.cpp
 
 Compiling TouchGFX/generated/fonts/src/Table_verdana_10_4bpp.cpp
 
 Compiling TouchGFX/generated/fonts/src/Kerning_verdana_20_4bpp.cpp
 
 Compiling TouchGFX/generated/fonts/src/FontCache.cpp
 
 Compiling TouchGFX/generated/fonts/src/Kerning_verdana_10_4bpp.cpp
 
 Compiling TouchGFX/generated/fonts/src/Font_verdana_10_4bpp_0.cpp
 
 Compiling TouchGFX/generated/fonts/src/CachedFont.cpp
 
 Compiling TouchGFX/generated/fonts/src/Table_verdana_40_4bpp.cpp
 
 Compiling TouchGFX/generated/fonts/src/Table_verdana_20_4bpp.cpp
 
 Compiling TouchGFX/generated/fonts/src/ApplicationFontProvider.cpp
 
 Compiling TouchGFX/generated/images/src/__designer/Blue_Buttons_Round_Edge_small.cpp
 
 Compiling TouchGFX/generated/images/src/__designer/Blue_Buttons_Round_Edge_small_pressed.cpp
 
 Compiling TouchGFX/generated/images/src/BitmapDatabase.cpp
 
 Compiling TouchGFX/generated/texts/src/TypedTextDatabase.cpp
 
 Compiling TouchGFX/generated/texts/src/Texts.cpp
 
 Compiling Middlewares/ST/TouchGFX/touchgfx/os/OSWrappers.cpp
 
 Compiling TouchGFX/target/STM32F7Instrumentation.cpp
 
 Compiling Core/Src/main.cpp
 
 Compiling TouchGFX/target/STM32F7TouchController.cpp
 
 Compiling TouchGFX/target/STM32F7DMA.cpp
 
 Compiling TouchGFX/target/STM32F7HAL.cpp
 
 Compiling TouchGFX/target/GPIO.cpp
 
 Compiling TouchGFX/target/HW_Init.cpp
 
 Compiling TouchGFX/target/BoardConfiguration.cpp
 
 In file included from Core/Src/main.cpp:53:0:
 
 Core/Src/main.cpp: In function 'int main()':
 
 Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.h:470:54: warning: ISO C++ forbids converting a string constant to 'char*' [-Wwrite-strings]
 
 { #name, (thread), (priority), (instances), (stacksz)}
 
 ^
 
 Core/Src/main.cpp:176:5: note: in expansion of macro 'osThreadDef'
 
 osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 4096);
 
 ^~~~~~~~~~~
 
 Compiling Middlewares/Third_Party/FreeRTOS/Source/croutine.c
 
 Compiling Middlewares/Third_Party/FreeRTOS/Source/list.c
 
 Compiling Middlewares/Third_Party/FreeRTOS/Source/tasks.c
 
 Compiling Middlewares/Third_Party/FreeRTOS/Source/queue.c
 
 Compiling Middlewares/Third_Party/FreeRTOS/Source/timers.c
 
 Compiling Middlewares/Third_Party/FreeRTOS/Source/portable/MemMang/heap_2.c
 
 Compiling Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1/port.c
 
 Compiling Drivers/BSP/STM32746G-Discovery/stm32746g_discovery.c
 
 Compiling Drivers/BSP/Components/ft5336/ft5336.c
 
 Compiling Drivers/BSP/STM32746G-Discovery/stm32746g_discovery_ts.c
 
 Compiling Drivers/BSP/STM32746G-Discovery/stm32746g_discovery_qspi.c
 
 Compiling Drivers/BSP/STM32746G-Discovery/stm32746g_discovery_sdram.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_cortex.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_dma.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_dma2d.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_gpio.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_dma_ex.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_i2c.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_i2c_ex.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_ltdc.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_nor.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_pwr_ex.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sdram.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sd.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_qspi.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_pwr.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_crc_ex.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_crc.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rtc.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rtc_ex.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_uart.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_fmc.c
 
 Compiling Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_sdmmc.c
 
 Compiling Core/Src/system_stm32f7xx.c
 
 Compiling Core/Src/freertos.c
 
 Compiling Core/Src/stm32f7xx_hal_msp.c
 
 Compiling Core/Src/stm32f7xx_hal_timebase_tim.c
 
 Compiling Core/Src/stm32f7xx_it.c
 
 Compiling ASM Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/gcc/startup_stm32f746xx.s
 
 Compiling Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.c
 
 Linking TouchGFX/build/bin/target.elf
 
 Producing additional output formats...
 
 target.hex - Combined internal+external hex
 
 intflash.elf - Internal flash, elf debug
 
 intflash.hex - Internal flash, hex
 
 extflash.bin - External flash, binary
 
 Done
 
 Flash
 
 make -f ../gcc/Makefile -j8 flash
 
 Converting images
 
 Linking TouchGFX/build/bin/target.elf
 
 Producing additional output formats...
 
 target.hex - Combined internal+external hex
 
 intflash.elf - Internal flash, elf debug
 
 intflash.hex - Internal flash, hex
 
 extflash.bin - External flash, binary
 
 /usr/bin/sh: C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ST-LINK_CLI.exe: No such file or directory
 
 gcc/Makefile:318: recipe for target '_extflash_' failed
 
 make[1]: *** [_extflash_] Error 127
 
 ../gcc/Makefile:50: recipe for target 'flash' failed
 
 make: *** [flash] Error 2
 
 Failed

HP_it
Senior II
December 25, 2019

Wouldn't it be a good idea to update the firmware on your ST-link first? press the big blue 'firmware upgrade' button and see if that works.

the examples in TouchGFX designer should work out of the box. do they?

SVict.1
Visitor II
May 27, 2020

Did you find the solution? if yes please post it. thanks