Skip to main content
AD�?b
Senior
December 11, 2020
Solved

STM32F746G-DISCO, TouchGFX

Hi

Problem.

  • There are two screens, S1 and S2.
  • The S1 has two buttons. GO to change screen to S2 and ON to set output pin.
  • The ON button state is sent to main.c.
  • I want to change the screen after pressing GO, but also the state of the ON button.

How to do it?

best regards

Andrzej

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
December 12, 2020

More options is dont create interactions, but write code directly to view.cpp in IDE ...

4 replies

MM..1
Super User
December 12, 2020

More options here , but in TouchGFX directly you can create serialized Interactions, mean when one interaction ends start second. Try use this...

AD�?b
AD�?bAuthor
Senior
December 12, 2020

Where's more options?

MM..1
MM..1Best answer
Super User
December 12, 2020

More options is dont create interactions, but write code directly to view.cpp in IDE ...

AD�?b
AD�?bAuthor
Senior
December 12, 2020

OK.