Skip to main content
This topic has been closed for replies.

6 replies

Karan 123
Senior
April 21, 2020

Hi,

Did you able to work on Hardware STM32F746G-DISCO with proper tool chain configuration ?

If Not, Please check attachment .

--

Karan

AD�?b
AD�?bAuthor
Senior
April 22, 2020

Thank you!

I will check and answer

Andrzej

chaaalyy
Senior II
April 21, 2020

Hi =) If you follow the steps from the video, everything should be fine. Does it run, if you comment out the "xQueueSend..." ? Anyway: You send the Message far more often, than you can handle it... You send every 1ms (more or less) and in model::tick() usually gets called with 60Hz ... I´m not used to XQueue, but i don´t see any external declaration of "poster" in model.cpp ...

AD�?b
AD�?bAuthor
Senior
April 22, 2020

Hi!

I changed the time but it did nothing.

The ( uint8_t poster ) declaration is in the Model.hpp file. Is that enough

Earlier I uncommented xQueueSend the program did not crash.

Now the program compiles without errors but there is a bad picture.

I have to start again. I'll write if I manage.

Thank you

Andrew