Skip to main content
This topic has been closed for replies.
Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
February 25, 2021

Hi,

Could you add the TouchGFX tag to your post ? This will increase the visibility.

The video you shared is a bit outdated. You should create a project from TouchGFX Designer with the application template for the STM32F746 disco board, then generate code. In your project folder you just need to double click on the cubdeIDE project in the /STM32CubeIDE folder to work with this toolchain.

/Romain

4 replies

Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
February 25, 2021

Hi,

Could you add the TouchGFX tag to your post ? This will increase the visibility.

The video you shared is a bit outdated. You should create a project from TouchGFX Designer with the application template for the STM32F746 disco board, then generate code. In your project folder you just need to double click on the cubdeIDE project in the /STM32CubeIDE folder to work with this toolchain.

/Romain

ADębs.1
ADębs.1Author
Senior
February 25, 2021

How to do it?

Karl Yamashita
Principal
May 6, 2021

I have uploaded a new video using the latest STM32CubeIDE 1.6.1 and TouchGFX 4.16.0

https://www.youtube.com/watch?v=Q-mfuzW6S-0

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source