Skip to main content
AD�?b
Senior
September 12, 2020
Solved

STM32F746G-DISCO, STM32CubeIDE 1.4.0, GFX 4.14.0 TUTORIAL https://www.youtube.com/watch?v=12KXreXaLp0&t=3s

Compiles OK.

I set the GFX screen to blue.

Loads the black screen into the STM32F746G-DISCO.

Why?

This topic has been closed for replies.
AD�?b
AD�?bBest answer
Senior
September 14, 2020

Yes I use.

I found the cause. McAfee Protection!

Thank you

2 replies

Alexandre RENOUX
Visitor II
September 14, 2020

Hello,

Did you try with the F746G-DISCO Application Template in the Designer ? We create these Application Templates for users to start off with a working project.

Also, you can try to compare the two projects and see if there is any difference.

/Alexandre

AD�?b
AD�?bAuthorBest answer
Senior
September 14, 2020

Yes I use.

I found the cause. McAfee Protection!

Thank you