Skip to main content
davidra7
Associate III
May 22, 2019 12:11 PM UTC
Question

STM32F746 nucleo communication to LCD with FMC

I am setting new LCD screen with parallel 8080 protocol ( screen controller is SSD1351 ), I am using ST CubeMX to generate code for fmc ( attached picture of the configuration ). My problem is when I try to write command my D0-D7 is always 0 and my D/C, WR and RD behaving wired, I think it is related with some configuration or incorrect way to send the command.

ST CubeMX configuration: https://i.stack.imgur.com/LFwSG.png

FMC init code:

/* FMC initialization function */

static void MX_FMC_Init(void)

{

FMC_NORSRAM_TimingTypeDef Timing;

/** Perform the SRAM1 memory initialization sequence

*/

hsram1.Instance = FMC_NORSRAM_DEVICE;

hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;

/* hsram1.Init */

hsram1.Init.NSBank = FMC_NORSRAM_BANK1;

hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;

hsram1.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;

hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_8;

hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;

hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;

hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;

hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;

hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;

hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;

hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;

hsram1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;

hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;

hsram1.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE;

hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE;

/* Timing */

Timing.AddressSetupTime = 2;

Timing.AddressHoldTime = 0;

Timing.DataSetupTime = 4;

Timing.BusTurnAroundDuration = 0;

Timing.CLKDivision = 0;

Timing.DataLatency = 0;

Timing.AccessMode = FMC_ACCESS_MODE_A;

/* ExtTiming */

if (HAL_SRAM_Init(&hsram1, &Timing, NULL) != HAL_OK)

{

Error_Handler( );

}

}

Because I use bank1 the adderss to write is 0x60000000

#define LCD_BASE_Addr ((uint32_t * )(0x60000000))

#define LCD_BASE_Data ((uint32_t *)(0x60000000|0x00000001))

My write command is

void LCD_SendCommand(uint8_t com){

*(__IO uint32_t*)(LCD_BASE_Addr) = com;

}

Command exmaple call

LCD_SendCommand(0xAF);

The result shown : https://i.stack.imgur.com/DTh2F.png

Small guide for scope configuration: on the left side there is signal names but they are not D0-D7 data signals. D1 - is CS D2- is D/C D3- is WR D4- is RD D5- is D0 (data)

My questions: 1. why it is generating 16 commands (16 times D/C)? 2. is my send command correct? 3. Where D0-D7 configured? In the CubeMX I save the D0-D7 configured as Data pins but not on FMC init.

Thanks for you help,

David

This topic has been closed for replies.