STM32f746 board[LTDC and I2C ] vs CUSTOM board[only LTDC] pin connection with LCD Display
Hello Touchgfx Team,
In STM32f746 disc board there is LTDC as well as I2C peripherals used for the LCD
Where as the custom board which I am using has only LTDC and there is no I2C peripheral connected to the LCD display.
Why does the I2C peripheral used in discovery board , is that used for controlling touch on the Display.
If so the Custom board which I have will it work by using only LTDC peripheral.
All LCD related features will they work with LTDC alone or need I2C as well?
Please let me know.
Thanks,
Upender.