Skip to main content
pradeepsysargus
Associate II
Jan 31, 2017 5:44 AM UTC
Question

STM32F4xx and character LCD not talking using I2C - HAL library

Posted on January 31, 2017 at 06:44

I am trying to make communication between

STM32F411RCT6 and character LCD

NHD-C0220BIZ-FS(RGB)-FBW-3VM using I2C protocol.

STM32 is the master and the LCD is slave device. I am using stm32cubemx and HAL libraries for this.

Following is my code so far:

#define LCD_ADDRESS 0x78

uint8_t commands[10] = {0x00,0x38, 0x39, 0x14,0x78,0x5e,0x6d,0x0c,0x01,0x06 };

uint8_t data[4] = { 0x40, 0x61, 0x62,0x63 }; // characters a,b,c to be displayed starting from RAM address 0x

HAL_StatusTypeDef halstatus = 0;

void Init_LCD()

{

halstatus = HAL_I2C_IsDeviceReady(&hi2c1,(uint16_t) (LCD_ADDRESS),2,100);

printf('halstatus1 = %d\r\n',halstatus);

halstatus = HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)LCD_ADDRESS, commands, 10, 100);

printf('halstatus2 = %d\r\n',halstatus);

}

void Show_LCD()

{

halstatus = HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)LCD_ADDRESS, data, 4, 100);

printf('halstatus3 = %d\r\n',halstatus);

}

int main(void)

{

HAL_Init();

SystemClock_Config();

MX_GPIO_Init();

MX_USART1_UART_Init(); MX_I2C1_Init();

Init_LCD();

Show_LCD();

while (1)

{ } }

I am getting output as:

halstatus1 = 0;

halstatus2 = 1;

halstatus3 = 1;

I was expecting characters a,b,c to be displayed on the LCD screen, which is not happening.

The

HAL_I2C_Master_Transmit() function fails with HAL_ERROR, it is sending 10 bytes first time and 4 bytes another time.

When I try to send just 2 command bytes usingHAL_I2C_Master_Transmit() instead of 10 bytes, halstatus2 is zero or HAL_OK, but it does not configure my LCD display.

Following is the C code of character LCD given in the data sheet:

/* Initializes the LCD panel. */

void init_LCD(void) { I2C_Start();

I2C_out( 0x78 ); // Slave address of the LCD panel.

I2C_out( 0x00 ); // Control byte: all following bytes are commands. I2C_out( 0x38 ); // 8-bit bus, 2-line display, normal instruction mode. delay( 10 );

I2C_out( 0x39 ); // 8-bit bus, 2-line display, extension instruction mode.

delay( 10 );

I2C_out( 0x14 ); // Bias set to 1/5.

I2C_out( 0x78 ); // Contrast set. I2C_out( 0x5E ); // Icon display on, booster on, contrast set. I2C_out( 0x6D ); // Follower circuit on, amplifier=1? I2C_out( 0x0C ); // Display on, cursor off. I2C_out( 0x01 ); // Clear display. I2C_out( 0x06 ); // Entry mode set to cursor-moves-right. delay( 10 );

I2C_Stop();

}

/* Writes a 10-char string to the RAM of the LCD. */

void show( unsigned char *text ) { int n;

I2C_Start();

I2C_out( 0x78 ); // Slave address of panel.

I2C_out( 0x40 ); // Control byte: data bytes follow, data is RAM data.

for( n = 0; n < 10; n++ ) {

I2C_out( *text ); text++; }

I2C_Stop();

}

void main(void) {

int i;

init_LCD();

show('HelloWorld');

while(1)

{} }

Please update me why

HAL_I2C_Master_Transmit() is failing with HAL_ERROR two times.

Am I doing wrong somewhere .. ?

Thanks,

#character-lcd #i2c-stm32f4xx #stm32cubemx #stm32f4
This topic has been closed for replies.

2 replies

EPera
Visitor II
Sep 25, 2018 12:47 PM UTC

I have the same problem and the address you use is a special address defined by i2c specs.

#define LCD_ADDRESS 0x78

Addresses from 0x78 to 0x7B define a address with 10 bits.

I'd like to know if there is a possibility to avoid the 10 bit address in i2c peripheral.

waclawek.jan
Super User
Sep 25, 2018 1:31 PM UTC

That display is based on ST7036, and the I2C address is 8-bit 0x78; that's 0x3C if seen as 7-bit address. The I2C standard does not recognize the 8-bit addresses.

JW