Skip to main content
Fran Marala
Associate II
October 8, 2020
Question

STM32F469I-DISCO. Screen using a custom container made-up for 16 checkbox, work in simulator but not in the hardware board.

Hi,

I'm developing an application using touchGFX Designer Version: 4.13.0, all is working correctly when you run Simulator in touchGFXDesingner tool, but when flashing in disco board the screen is fridge and I have to reset the system, again and again the same problem. I have tested that if I use only 4 checbox widget instead of 16 all is working properly, more than four return the same problem.

Waiting for your help

Regards

Fracncisco

This topic has been closed for replies.

2 replies

Fran Marala
Associate II
October 9, 2020

Hi, I have tested tat in version 4.14 this bug is fixed

Fran Marala
Associate II
October 9, 2020

Sorry, unfortunately the problem still appear with version 4.14.

Attached below both the right option running is simulator and the bug running in dtn32469I-DISCO

0693W000004JEX8QAO.png

0693W000004JEZ4QAO.png

As you can see in the second picture, the screen referred is appearing from the west, but the screen is fridge a that point.