Skip to main content
moritz2
Visitor II
Jul 12, 2016 11:08 PM UTC
Question

STM32F469 higher resolution display

Posted on July 13, 2016 at 01:08

Hello everyone,

I want to use a 1280x120 display (16bit parallel RGB interface) with a STM32F469.

The datasheet says that it can only support a maximum resolution of 1024x768.

The horizontal resolution of my display is a bit higher, but my total bandwith schould be much less, because the vertical resolution is so low.

Is it possible somehow?

Thanks for your help,

Moritz

#stm32 #lcd #tft #stm32f469
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Jul 13, 2016 12:35 AM UTC
Posted on July 13, 2016 at 02:35

Is it possible somehow?

Probably, its a matter of total memory size, bandwidth, and width of control registers. If you don't violate the first two, it will come down to the last. Make sure there is a >10-bit register describing the width of the screen raster.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..