Skip to main content
JMana.637
Associate
Oct 30, 2019 10:51 AM UTC
Solved

STM32F429ZE only has two options available (RGB666 and RGB565) in the LTDC configuration, there should be the RGB888 option according to the datasheet.

Hi,

I'm not sure whether this is a bug in the Cube or whether I'm missing out something. I tried opening the F439 in the Cube and it has the 24-bit RGB option. Just to check while I was there I searched for the LTDC_B0 pin and found it on PE4, so I went back to my F429 window and sure enough, when I click on the PE4 pin, it can be configured as LTDC_B0, yet that would only be possible in the 24-bit RGB888 mode. So I'm confused.

I'm on 5.3.0. I went through the bug fixes included in the recent 5.4. release but didn't find my problem.

I guess it wouldn't be a problem to generate the code for the F439 and copy it over but I'm still not sure whether my micro supports it and I have no way of testing it rn. My display only supports the 18-bit RGB but I want to replace it with slightly different one which in turn only supports the 24-bit...

Thank you for your suggestions.

This topic has been closed for replies.
Tilen MAJERLE
Tilen MAJERLEBest answer
ST Employee
Oct 30, 2019 3:28 PM UTC

Hello @JMana.637​ ,

LQFP144 package does not support RGB888 format. You would need to go to higher package instead.

Best regards,

Tilen

2 replies

Tilen MAJERLE
Tilen MAJERLEBest answer
ST Employee
Oct 30, 2019 3:28 PM UTC

Hello @JMana.637​ ,

LQFP144 package does not support RGB888 format. You would need to go to higher package instead.

Best regards,

Tilen

JMana.637
JMana.637Author
Associate
Oct 30, 2019 4:18 PM UTC

I see, I didn't notice it in the datasheet then.

Thank you!