Skip to main content
ferhatyol-23
Senior
Apr 3, 2014 9:27 AM UTC
Question

STM32F429 Discovery LTDC with DCMI?

Posted on April 03, 2014 at 11:27

Hello Friends. 

I want to connect the camera to the STM32F429 Discovery. I need to use DCMI module but I can't use with LTDC hardware. Because LTDC with DCMI using some common pins.(For example; PA4 = DCMI_HSYNC=LTDC_VSYNC)

 How do I use the DCMI and LTDC hardware simultaneously?

#ltdc #dcmi
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Apr 3, 2014 11:40 AM UTC
Posted on April 03, 2014 at 13:40

How do I use the DCMI and LTDC hardware simultaneously?

You clearly can't use them ''simultaneously'', you need to look for a board with a higher pin count device.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
stm322399
Senior
Apr 3, 2014 11:48 AM UTC
Posted on April 03, 2014 at 13:48

I don't know what is *the* camera.

AFAIK, DMCI can deal with synchronization embedded into data (see RM).

If the camera is compatible, you still have a chance to make LTDC and DMCI working together, without DMCI_HSYNC.

ferhatyol-23
Senior
Apr 3, 2014 12:46 PM UTC
Posted on April 03, 2014 at 14:46

hi,

I use the OV9655 camera module. The camera doesn't work without the HSYNC and VSYNC signals.

I have to use the camera with the software interface.