Skip to main content
matej2
Associate
February 5, 2020
Solved

STM32F429 discovery board

Has anyone been able to create a working project with CubeMX 5.5 and TouchGFX 4.13?

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
March 31, 2020

Did you check the Application template from the designer?

There's a new version 3 up that supports CubeMX 5.5!

/Martin

3 replies

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
March 31, 2020

Did you check the Application template from the designer?

There's a new version 3 up that supports CubeMX 5.5!

/Martin

MKsen.1
Associate II
April 1, 2020

I did at first, but it wasn't there. Now I see that there is a new template version there. Thanks for posting this, and I will give it a try.

Matej

MKsen.1
Associate II
April 15, 2020

I have tried it out and if you are using the template screen transitions are not working on device (project built with cube IDE), but are working fine in the TouchGFX Simulator. Is there something that needs to be enabled?

Thx Matej