Skip to main content
Caan
Associate III
Jan 24, 2025 1:53 PM UTC
Solved

STM32F429 Custom TFT Board With 4.3" TFT

I have designed a STM32F429 Custom TFT Board With 4.3" TFT it is based on 32F429IDISCOVERY MCU + RAM + 4.3" TFT in 16 bit mode and I'm using TouchGFX.

I have few questions.
1) It is possible to remove External RAM from the System.
2) How to limit RAM Usage so as to use the internal MCU RAM only

This topic has been closed for replies.
LouisBBest answer
ST Employee
Feb 4, 2025 9:21 AM UTC

Hello @Caan,

1) That's out of the touchgfx scope, this more related to linker script/ compilation of your project, your board as very little ram so it's useless.

2) You can try to do some optimization here and there but considering the size of the framebuffer, that's very small savings.

Best regards,

Louis BOUDOST Software Engineer | TouchGFX

8 replies

mƎALLEm
ST Technical Moderator
Jan 24, 2025 2:15 PM UTC

Hello,

Are you using TouchGFX for this case?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Caan
CaanAuthor
Associate III
Jan 24, 2025 2:17 PM UTC

Hello,
         Yes, I am using the Touchgfx.

mƎALLEm
ST Technical Moderator
Jan 24, 2025 2:22 PM UTC

Ok. Need to tell that in the first post because the answer may differ and your question could be generic not specific (related to TouchGFX).

I'm editing it then ..

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Caan
CaanAuthor
Associate III
Jan 24, 2025 2:30 PM UTC

I did specified that " I have designed a STM32F429 Custom TFT Board With 4.3" TFT it is based on 32F429IDISCOVERY MCU + RAM + 4.3" TFT in 16 bit mode and I'm using TouchGFX ".
 I would like to know your thoughts on using internal RAM as Frame buffer.

mƎALLEm
ST Technical Moderator
Jan 24, 2025 2:34 PM UTC

@Caan wrote:

I did specified that " I have designed a STM32F429 Custom TFT Board With 4.3" TFT it is based on 32F429IDISCOVERY MCU + RAM + 4.3" TFT in 16 bit mode and I'm using TouchGFX ".


No. That was my edit ;)

SofLit_0-1737729256293.png

One of the TouchGFX expert can help you on that.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Caan
CaanAuthor
Associate III
Jan 24, 2025 3:43 PM UTC

Alright, Thank you for the help.