Skip to main content
Associate
Dec 3, 2023 12:40 PM UTC
Question

STM32F401-RE with X-NUCLEO-GFX01M2 ($AZ2)

Has anyone some sample-projects to integrate these 2 hardware?

I'd need the detailed procedure to use the display with this board.

Thanks in advance.

This topic has been closed for replies.

4 replies

STTwo-32
ST Technical Moderator
Dec 3, 2023 3:26 PM UTC

Hello @GPioldi and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you use the examples of the X-CUBE-DISPLAY Expansion Package. Those examples are tested using the NUCLEO-G071RB and NUCLEO-WB55RG.  But you can adapt them to the NUCLEO-F401-RE.

Best Regards

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
GPioldiAuthor
Associate
Dec 3, 2023 3:28 PM UTC

Sorry but I don't know how to adapt them to NUCLEO-F401-RE... any suggestion / explanation? Thanks, Giuliano.

STTwo-32
ST Technical Moderator
Dec 4, 2023 5:10 PM UTC

Hello @GPioldi 

You can start by understanding how this works. Then, you can make it compatible with your NUCLEO-F401-RE. You have to give attention to differences in hardware, peripheral availability, firmware, security, and tools.

You can also use the NUCLEO-G071RB or the NUCLEO-WB55RG with the examples to start if you are not ready to do an example migration.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.