Skip to main content
DMavr.1
Visitor II
April 12, 2020
Question

STM32CubeIDE v1.3.0 + TouchGFX v4.13.0 + CubeMX 5.6.0 -- Issue Compiling when using latest versions of those apps together.

Hi!

Given the circumstances, I've finally found time to learn the STM32 dev environment. I have a STM32F769iDisco board.

I've successfully used TouchGFX v4.13.0 to start a new project with a simple interface (background and button). I can compile, simulate and run on target.

I've also been able to use CubeMX to open the ICO file and to modify board settings and then compiling & running using TouchGFX.

The issues begin when I try and debug using STM32CubeIDE. I open the project in a new workspace, build without errors, but when I try and run or debug I get an error.

In the console I get:

STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled
 
Waiting for debugger connection...
Debugger connected
Debugger connection lost.
Shutting down...

And a "Problem Occurred" Alert with the following error:

Error in final launch sequence:
 
Failed to execute MI command:
load C:\\TouchGFXProjects\\ScreenMaskingController\\STM32CubeIDE\\Debug\\STM32F769I_DISCO.elf 
 
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\ScreenMaskingController\\STM32CubeIDE\\Debug\\STM32F769I_DISCO.elf 
 
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\ScreenMaskingController\\STM32CubeIDE\\Debug\\STM32F769I_DISCO.elf 
 
Error message from debugger back end:
Load failed
Load failed

The same project builds fine with TouchGFX but not via the IDE. Why?

Is there a way to change the IDE to use the same compiler/programmer settings TouchGFX is using?

Thanks.

This topic has been closed for replies.

9 replies

Martin KJELDSEN
Principal III
April 29, 2020

Hi,

Are you still having this issue?

aponski
Associate
December 20, 2020

DMavr.1 how did you solve this isssue?

GOtté.1
Visitor II
January 14, 2021

I encounter the same problem. Anybody an idea how to fix this?

aponski
Associate
January 14, 2021

Me too

Martin KJELDSEN
Principal III
January 18, 2021

​Is an external flashloader configured for the project? These versions are pretty old now - what are your current toolchain versions?

Some of the ATs were missing flashloader configuration which would cause this. But should have been fixed.

GOtté.1
Visitor II
January 18, 2021

I'm working with TouchGFX 4.16, STM32CubeIDE 1.51 (latest versions) on a NUCLEO-G071RB + X-NUCLEO-GFX01M1 board.

I opened the one sample project available for this board combo in CubeMX, uploaded it to the board without any problem.

Then I opened the project in CubeIDE, compiled without any problem, but uploading/running is returning these errors:

Error in final launch sequence:
 
Failed to execute MI command:
load C:\\TouchGFXProjects\\GFX01_Test01\\STM32CubeIDE\\Debug\\STM32G071_NUCLEO.elf 
 
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\GFX01_Test01\\STM32CubeIDE\\Debug\\STM32G071_NUCLEO.elf 
 
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\GFX01_Test01\\STM32CubeIDE\\Debug\\STM32G071_NUCLEO.elf 
 
Error message from debugger back end:
Load failed
Load failed

And there is no external flashloader configured.

When I enable the external flashloader (S25FL032P_STM32G071B-NUCLEO, 0x90000000, SPI_FLASH, S25FL032P_STM32G071B-NUCLEO.stldr)

This is returned:

Error in final launch sequence:
 
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (-2147155971) Unknown. Please check power and cabling to target.

GOtté.1
Visitor II
January 18, 2021

Maybe it's related, but when I build the release in STM32CubeIDE, the .bin file is >2GB!

Is this because of this in the linker script:

SPI_FLASH (r)   : ORIGIN = 0x90000000,  LENGTH = 8M

Martin KJELDSEN
Principal III
January 19, 2021

It's because .bin files do not contain notions of memory ranges, so it has to contain all the data from 0x0-0x90000000+8M. Disable bin file generation if you don't need it - You probably just want the .elf or .hex

GOtté.1
Visitor II
January 19, 2021

A small update. I convert the generated .elf file to a .hex file (the .bin is way too big) : arm-none-eabi-objcopy -O ihex STM32G071_NUCLEO.elf STM32G071_NUCLEO.hex

Then I programmed the board by using "ST-Link Utility" and the external loader file (MX25L6433F_STM32G071B_NUCLEO.stldr) from the folder "en.X-CUBE-DISPLAY_1_0_0\Utilities\PC_Software\ExternalLoader".

And this is working fine, so the building in STM32CubeIDE is fine, only the uploading to the board is failing.