Skip to main content
Acai.1
Associate II
Dec 16, 2019 2:51 AM UTC
Question

STM32Cube_FW_L4_V1.14.0, cannot find TouchGFX source code of 32L4R9IDISCOVERY ! Where can I get it ?

..

This topic has been closed for replies.

11 replies

Martin KJELDSEN
Principal III
Dec 16, 2019 12:09 PM UTC

Please be more specific. Are you talking about a specific demo or example in the Cube FW packs?

/Martin

Acai.1
Acai.1Author
Associate II
Dec 16, 2019 3:08 PM UTC

Hi Martin,

Acai.1
Acai.1Author
Associate II
Dec 16, 2019 3:09 PM UTC

STM32Cube_FW_L4_V1.14.0\Projects\32L4R9IDISCOVERY\Demonstrations\TouchGFX without source code.

Martin KJELDSEN
Principal III
Dec 17, 2019 9:35 AM UTC

I'll check if this is something i can share.

Acai.1
Acai.1Author
Associate II
Dec 16, 2019 3:11 PM UTC

if using TouchGFX 4.12.3 Designer to generate the "TouchGFX Watch" project for 32L4R9IDISCOVERY, it has IAR and gcc only, is there any Keil project ?

Martin KJELDSEN
Principal III
Dec 17, 2019 9:34 AM UTC

No Keil project, but you could probably make it yourself.

Acai.1
Acai.1Author
Associate II
Dec 16, 2019 3:12 PM UTC

More, any Good TouchGFX tutorial for helping us to change the LCD of 32L4R9IDISCOVERY to customer's one ?

Martin KJELDSEN
Principal III
Dec 17, 2019 9:37 AM UTC

No specific guides for that. If you have any concrete questions i'd be happy to help. Generally:

1) Update hardware configuration accordingly

2) Ensure that TouchGFX is driven by events from this new display. If this display is the same display interface you could get some inspiration from your existing project. If MIPI DSI do you want to run in adapted command mode or video mode? etc.

3) Update TouchGFX GUI according to new dimensions

/Martin

Acai.1
Acai.1Author
Associate II
Dec 17, 2019 9:29 AM UTC

"TouchGFX Watch" can be run up on EVB 32L4R9IDISCOVERY, thank you.

Acai.1
Acai.1Author
Associate II
Dec 17, 2019 9:30 AM UTC

Here comes next question, how to modify it to use customer's 454x454 MIPI LCD ? any application note ? thank you !

Martin KJELDSEN
Principal III
Dec 17, 2019 9:39 AM UTC

Wrote a general overview a few posts up.

/Martin