STM32Cube_FW_H7_V1.3.2 migrate to STM32Cube_FW_H7_V1.8.0 give problems with SDRAM, FMC and LTDC ...
Hi
I did buy a https://www.waveshare.com/wiki/OpenH743I-C and they provide some sample codes...
They are all made in STM32Cube_FW_H7_V1.3.2 and works fine when i do compile in Stm32cubeide.
BUT ...when i do say MIGRATE to STM32Cube_FW_H7_V1.8.0 i got problems with LTDC, SDRAM and FMC.
Nothing happend on the screeen and it seems like i got hardware failure when trying to write to 0xD0000000 whitch and the FMC bank 2 as the SDRAM are connected to.
Do anyone have a glue ...WHat have changed in HAL drivers files from 1.3.2. to 1.8.0 ?
Thanks
Hjalmar