Skip to main content
crusso9
Associate
Nov 23, 2012 9:07 AM UTC
Question

STM324xG LCD: GRAM Write Direction Values

Posted on November 23, 2012 at 10:07

Hello,

I was playing with the LCD interface of the STM3240G-Eval and I found that before writing on the GRAM I can set the GRAM Direction using following code: LCD_WriteReg(LCD_REG_3, <myValue>);

Looking at the source code of stm324xg_eval_lcd.c I found that I can set this register to three different values which are 0x1018, 0x1008, 0x1030:

0x1018 means Horizontal Increment, Vertical Decrement and address is updated in vertical direction;

0x1008 means Horizontal Decrement, Vertical Decrement and address is updated in vertical direction;

I didn't find in the manual and in the source code any information about the value 0x1030.

I tried to set the write direction to 0x1030 and I found out that the lcd is refreshed with flickering.

What does it means setting LCD_REG_3 register to 0x1030 ?

Thank you so much.

#lcd #stm3240g
This topic has been closed for replies.

1 reply

waclawek.jan
Super User
Nov 23, 2012 4:01 PM UTC
Posted on November 23, 2012 at 17:01

The GLCD's control chip is Ilitek ILI9320, try to locate a datasheet for it and check yourself.

JW