Skip to main content
Faisal Haque
Associate II
May 24, 2020
Solved

STM32 dual core MCU

I am developing a board based on STM32H747XIH6 MCU. When TouchGFX support will be added in additional software section of CubeIDE?

This topic has been closed for replies.
Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
July 2, 2021

Hi,

TouchGFX 4.17 is now live with dual core support and along a new release of the TouchGFX Board Setup (new name for "Application template") for the STM32H747-disco board based on STM32CubeMX and with a STM32CubeIDE project.

/Romain

5 replies

Alexandre RENOUX
Visitor II
May 25, 2020

Hello,

We currently cannot give you an answer yet because this is something related to CubeMX. So as soon as CubeMX supports the STM32H747, we will create the corresponding Application Template that will support CubeIDE.

This is something that got requested quite a few times so we'll try to push it so that the release comes as soon as possible.

Sorry for the inconvenience.

/Alexandre

Martin KJELDSEN
Principal III
May 27, 2020

Hi,

Additional Software support for dual cores should be in by Q4 this year, according to the CubeMX team.

/Martin

Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
July 2, 2021

Hi,

TouchGFX 4.17 is now live with dual core support and along a new release of the TouchGFX Board Setup (new name for "Application template") for the STM32H747-disco board based on STM32CubeMX and with a STM32CubeIDE project.

/Romain

SFuch.1
Associate II
July 22, 2021

I have a STM32H747-Disco. How do I select that the GUI runs on the M4 core instead of the M7 which is normally used?

YSN
Associate III
July 22, 2021

You need to download touchgfx library for M4 in Manage softwares link under STM32Cube IDE.