Skip to main content
APort
Associate III
November 25, 2019
Question

STemWin5.44 lib missing GUI_SPLINE functions

Hello,

Latest version of STemWin as included in STM32Cube_FW_L4_V1.14.0 apparently missing GUI_SPLINE_* functions in the provided *.a libs but they are listed in header file (GUI.h) - which causes linking error.

We are working with STemWin_CM4_wc32_ot_ARGB.a in particular but others are missing it as well.

This is very important feature for us.

Is there newer version, or version with this feature working?

Thanks in advance

This topic has been closed for replies.

1 reply

CSage
Visitor II
May 13, 2020

Hej,

Could you solve this issue?

I´m using STM32Cube_FW_F4_V1.24.2. This results into the same issue. I´m also using the same lib STemWIN_CM4_OS_wc32_ot_ARGB.a.