Skip to main content
nicolas b
Associate III
Oct 26, 2018 7:40 AM UTC
Question

STemWin's simulator, color problem.

Hello,

We have facing troubles with STemWin's simulator.

Our embedded project creates the GUI driver like this:

void LCD_X_Config(void) {
 
 GUI_DEVICE_CreateAndLink(GUIDRV_LIN_16, GUICC_M565, 0, 0);
 ...
 } 

 Our simulator project creates it like this:  

Our simulator project creates it like this:
 void LCD_X_Config(void) {
 GUI_DEVICE_CreateAndLink(GUIDRV_WIN32, GUICC_M565, 0, 0);
 
 ...
 }

Both project uses the same GUIConf.h:

   

 #ifndef GUICONF_H
 #define GUICONF_H
 
 // The following settings are from STewmWin application note
 // See https://www.st.com/content/ccc/resource/technical/document/application_note/54/c9/95/42/8c/0b/43/69/DM00089670.pdf/files/DM00089670.pdf/jcr:content/translations/en.DM00089670.pdf
 // FAQ question 2 "What is the STemWin Library configuration(during the binary generation) ?"
 
 #define GUI_DEFAULT_FONT &GUI_Font6x8
 #define GUI_NUM_LAYERS 2
 #define GUI_SUPPORT_TOUCH (1)
 #define GUI_SUPPORT_MOUSE (1)
 #define GUI_WINSUPPORT (1)
 #define GUI_SUPPORT_MEMDEV (1)
 #define GUI_SUPPORT_DEVICES (1)
 #define BUTTON_REACT_ON_LEVEL (1)
 #define GUI_MEMDEV_SUPPORT_CUSTOMDRAW (1)
 #define GUI_USE_ARGB (1)
 
 #endif

Projects links against the following libraries:   

  • Embedded --> STemWin540_CM4_OS_GCC_ARGB.a
  • Simulator --> STemWin540_WIN32_ARGB.lib

All colors (bitmaps, texts, drawings) are correct on board while they are inverted on the simulator. On board, using GUICC_565 instead of GUICC_M565 inverts the colors and we get the same results as the simulator. Nevertheless, on the simulator, using GUICC_565 instead of GUICC_M565 has no effect.

At the end of the day, colors are always wrong on the simulator. What can we do to fix this?

Best regards,

Nicolas.

This topic has been closed for replies.