Skip to main content
Zach Neveu
Associate
Oct 10, 2017 5:33 PM UTC
Question

STEmWin not Displaying but LTDC Works

Posted on October 10, 2017 at 19:33

I am using an STM32F439BIT processor and developing in Keil uVision 5.  My goal is to make a touchscreen GUI for a VGA resolution touchscreen.  I have implemented STEmWin to the best of my abilities, using the LIN32 Driver (which should work with my touchscreen).  Using the hltdc.Init.Backcolor.Red/Green/Blue elements in LCD_LL_Init() I am able to set a solid color to the screen.  When I begin calling STEmWin functions (GUI_Clear(), GUI_DispStringAt(), etc.), nothing is printed to the screen.

Has anyone experienced this?  Anyone have insight into some common causes for this or what I may have missed?

Thanks!

#gui #display #touchscreen #stemwin
This topic has been closed for replies.

4 replies

Vangelis Fortounas
Associate II
Oct 11, 2017 3:21 PM UTC
Posted on October 11, 2017 at 17:21

Hello!

did you enabled CRC module? Its essential to work the driver.

Zach Neveu
Associate
Oct 11, 2017 6:39 PM UTC
Posted on October 11, 2017 at 18:39

HAL_CRC_MODULE_ENABLED is defined in stm32f4xx_hal_conf.h, and __HAL_RCC_CRC_CLK_ENABLE() is called before any GUI functions are called, so yes, I believe the CRC module should be enabled.  Is there anything else you can think of that may be causing the problem?

Thanks for your help!

Vangelis Fortounas
Associate II
Oct 11, 2017 6:57 PM UTC
Posted on October 11, 2017 at 18:57

Which LCD type you use?

LIN driver is for direct access to video memory only

GUI functions like GUI_DispStringAt use commands also , like SetWindowSize .