Skip to main content
zhao yongchao
Associate
May 23, 2017 4:46 AM UTC
Question

STemWin create QR_Code

Posted on May 23, 2017 at 06:46

Hi.

I'm using STemWin 5.28.

Today i was reading web page in seeger web. I find that  the lastest EMWin version is V5.40 .U

nbelievable,I find the function 

in the chapter '2-D  Graphic Library' GUI_QR_Creat(), GUI_QR_Delete()....

Now ,Which version of STemWin support QR_Code ? HOW can i get the lastest version?  

I'm using STM32f103vet6.

Best regards.

#qr_code #stemwin
This topic has been closed for replies.

2 replies

ST Technical Moderator
May 30, 2017 12:02 PM UTC
Posted on May 30, 2017 at 14:02

Hi

yongchao.zhao

,

QR-Codes functionadded in the STemWinversion 5.

Today,

the

STemWin-library is based on version V5.28 for the last version of STM32CubeF1 V1.4.0.

So,you can't use the

QR-Codes functions

since it is not available in the STemWin 5.28 with the last firmware package.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
zhao yongchao
Associate
Jun 1, 2017 3:51 AM UTC
Posted on June 01, 2017 at 03:51

Thank you for your help. I hope ST updates the lib as quickly. Now i only use the libqrencode written by fukuchi.  

 Best regards!