Skip to main content
MRedd.3
Associate II
Aug 12, 2022 11:30 AM UTC
Question

ST emwin library issue

We are using the emWIN library to display the images, but we are having problems. The initial screens 2 are displaying, but when you enter a specific screen, the display module does not respond.

We can't figure out what's wrong because it's structing the display.

Is this a memory problem with the controller 2MB flash 320 kb ram?

This topic has been closed for replies.

2 replies

ST Technical Moderator
Aug 31, 2022 7:51 PM UTC

Hello @MRedd.3​ ,

Could you please precise which board are you using ?

Are you enabled clock for CRC module ?

The display issue may be caused by one of the following:

 - Stack size is too low.

 - Wrong initialization of the display controller.

 - Wrong configuration of the display interface. 

Pease note that STemWIN requires quite a lot of RAM to just run itself. Actual RAM required for STemWIN depends on number of widget, fonts, features, etc.

I advise you this AN4323 "Getting started with STemWin Library" Application note may be helpful.

You can refer to one of the many STemWin examples under STM32CubeXX package and get inspired from them:

Example: STM32Cube_FW_F4_VX.X.X\Projects\STM324x9I_EVAL\Applications\STemWin, it can be very useful.

Hope my answer helped you!

When your question is answered, please close this topic by choosing Select as Best.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
Aug 31, 2022 8:01 PM UTC

>>Is this a memory problem with the controller 2MB flash 320 kb ram?

Debug on the probability that it is not.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..