Skip to main content
Associate II
Feb 19, 2024 4:41 AM UTC
Solved

ST boards and 10" touch screens?

Hello people.

First of all... I haven't worked with screen displays before, sorry if this post sounds dumb:

Now that I said the above:

I want to interact with any ST board GPIO through GUI buttons. I also want to do this on a "big" touch screen with great quality and not the 2-3" LCD screens that usually come with the boards.

1. Where can I find 10" LCD screens with great quality for this purpose? 

2. Which IDE will be better to draw the GUI? I have seen many, some are free and some are not (I use CubeIDE for everything not related to screens).

3. How can I communicate the GUI buttons with any ST board? Is it by I2C? Or I should instead use the GPIO of the board that runs the screen?

I hope I made myself clear enough to get pointed to the right direction.

Thanks for your time.

 

This topic has been closed for replies.
ST Employee
Feb 21, 2024 9:23 AM UTC

Hello @Lalogarcia91 ,

Riverdi offers boards with large displays with great quality which are accompanied by STM32 MCUs. Having those boards, then you can use TouchGFX to develop your GUI easily. TouchGFX provides you the necessary tools and settings for handling the communication between the GPIOs and the GUI. 
There are plenty of tutorials and documentations to help you get started with TouchGFX. You can also continue editing your project in STM32CubeIDE. 

Please take a look at the available documentations, and if you needed more help, don't hesitate to ask.

Best regards,

Mohammad MORADIST Software Developer | TouchGFX

10 replies

ST Employee
Feb 21, 2024 9:23 AM UTC

Hello @Lalogarcia91 ,

Riverdi offers boards with large displays with great quality which are accompanied by STM32 MCUs. Having those boards, then you can use TouchGFX to develop your GUI easily. TouchGFX provides you the necessary tools and settings for handling the communication between the GPIOs and the GUI. 
There are plenty of tutorials and documentations to help you get started with TouchGFX. You can also continue editing your project in STM32CubeIDE. 

Please take a look at the available documentations, and if you needed more help, don't hesitate to ask.

Best regards,

Mohammad MORADIST Software Developer | TouchGFX
Andrew Neil
Super User
Apr 9, 2024 9:34 AM UTC

SmartEmbedded is another one doing displays (up to 10.1") accompanied by STM32 MCUs:

https://smartembeddeddisplay.com/

https://smartembeddeddisplay.com/wp-content/uploads/2022/11/SE-Product-overview-NOV.2022-ver-1.3-Final-08112022.pdf

 

Another possibility would be to use something like a Raspberry Pi with a large display - either to replace the STM32, or to communicate with an STM32.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
Apr 9, 2024 3:50 PM UTC

MikroE and GHI Electronics might be worth a look too.

Riverdi seems a reasonable mix, without trying to kitchen-sink the problem. Very difficult, nigh impossible, to make a perfect board for every customer, they always want that one other thing..

I'd look for a board that hits 85% of the desired function at a suitable price point, vs DIY, and then using and interface to a custom daughter board to cover the other 15%. Determine your trade-offs vs costs, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Employee
Mar 15, 2024 12:31 PM UTC

Hello again @Lalogarcia91 ,

Have you managed to get your project going?

Mohammad MORADIST Software Developer | TouchGFX
Associate II
Apr 9, 2024 2:55 PM UTC

Oh, Hello Mohammsd.. So sorry for the late reply. I was on vacation at this time.

I got in contact with Riverdi and they point me in the right direction on which disolay screen to get. And I'm getting one on the next weeks, since I'm still working on another part of the project (commercial product). I hope to ise Riverdi screen once I start making the tests on the next weeks.

 

Thanks a lot.

Andrew Neil
Super User
Apr 9, 2024 3:00 PM UTC

Time to mark the solution, then?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
Mar 15, 2024 1:25 PM UTC

Usually not about size, but resolution.

Most of the STM32 MCU are limited to around 1388x768 (or about 1.0-1.2 Mpixel), due to bandwidth constraints.

Several vendors that specialize in bare panels, other in subsystems, shouldn't be hard to narrow down

RGB screens will need MCU with lots of pins. The MIPI/DSI displays need less pins, but are usually a different model of STM32, a differentiation for licencing / IP purposes.

High resolution you'll want wider memories, 32-bit data path, and again more pins. And at these resolutions at least 8MB for frame buffers, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
Mar 15, 2024 5:00 PM UTC

> How can I communicate the GUI buttons with any ST board? Is it by I2C?

Yes, according to the Riverdi documentation their ilitek touch screen interface to STM32 is I2C with interrupt pin. See here.

STM32 pins are also routed to the extension connector of the board. Wire on it anything you like.

 

ST Employee
Apr 9, 2024 9:12 AM UTC

I'm closing this ticket due to inactivity for a long time

Best regards,

Mohammad MORADIST Software Developer | TouchGFX