Skip to main content
Associate III
Jun 28, 2025 12:39 PM UTC
Question

Some problems about using dynamic bitmap on STM32N6570-DK

I am using TouchGFX to design GUI, and I want to use a dynamic bitmap to show an image captured by the camera. The camera is about 600*480 size. But I set the CacheAddress as following, and It turns out that the GUI cannot run properly. Is there any problem with it? 

uint16_t* const cacheStartAddr = (uint16_t *)0xC0008000;
const uint32_t cacheSize_own = 0x100000; //1 MB, as example
Bitmap::setCache(cacheStartAddr, cacheSize_own, 1);

This topic has been closed for replies.

6 replies

GaetanGodart
ST Employee
Jun 30, 2025 10:50 AM UTC

Hello @Z-YF ,

 

Are you able to make your project work without the dynamic bitmap first?

What is the exact format of the camera's output?

What do you mean by "the GUI cannot run properly", what is happening exactly?

Please read this article to use dynamic bitmap : https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/dynamic-bitmaps

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Z-YFAuthor
Associate III
Jun 30, 2025 10:53 AM UTC

You know, my main concern is where I can allocate the bitmap cache. Because there is no SDRAM on the N6-DK board.

GaetanGodart
ST Employee
Jun 30, 2025 12:28 PM UTC

The STM32N6570-dk has 4.2 Mbytes of contiguous SRAM, could you place the bitmap cache there?

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
ST Technical Moderator
Jul 31, 2025 6:29 AM UTC

Hello @Z-YF.

The TBS for STM32N6570-DK available in TouchGFX Designer is configured to support a bitmap cache next to the framebuffers in internal SRAM.

TouchGFX Demo 7 uses dynamic bitmaps in the video and text demo. You can try importing TouchGFX Demo 7 to see how it is used. The bitmap cache setup is done in FrontendApplication.cpp and looks like this:

#include <gui/common/FrontendApplication.hpp>

#if !defined(NO_BITMAP_CACHE)
LOCATION_PRAGMA_NOLOAD("TouchGFX_Framebuffer")
uint16_t bitmapCacheBuffer[800 * 480 + 800] LOCATION_ATTRIBUTE_NOLOAD("TouchGFX_Framebuffer");
#endif

FrontendApplication::FrontendApplication(Model& m, FrontendHeap& heap)
 : FrontendApplicationBase(m, heap)
{
 HAL::getInstance()->setFrameRateCompensation(true);

#if !defined(NO_BITMAP_CACHE)
 Bitmap::setCache(bitmapCacheBuffer, sizeof(bitmapCacheBuffer), 10);
#endif
}

You can, of course, also use the PSRAM available on the STM32N6570-DK for the bitmap cache. However, make sure to configure the MPU correctly for this memory region then. You can use the MPU configuration for the framebuffer region as reference.

Best regards,
Johan