Skip to main content
RReta.1
Associate II
July 13, 2021
Solved

[Solved] Typography wildcard, how to add punctuation char(s)?

Most of the sample shows how to add these ranges to the Wildcard Range

0-9,A-Z,a-z

How does one add punctuation chars into the Typography using TouchGFX designer?

. period
? question mark
! exclamation point
.. etc

Adding it as comma separators in Wildcard Ranges does not work.

Do we need to do it using the other columns? If so what is the difference between "Wildcard Characters" and "Widget Wildcard Characters"?

Also, with these being generated as glyphs, am I right to think that Wildcard ranges for larger point fonts will consume more code space? (i.e. 15pt vs 32pt fonts of the same typography)

Thanks for everyone's time

This topic has been closed for replies.
Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
July 14, 2021

Hello RReta.1,

You should put your punctuation characters in Wildcard Characters. In general the user does not use Widget Wildcard Characters.

For more information on Text handling, I highly recommend you to check the documentation website

Here is an extract :

Wildcard Characters:

Characters that should be available to display in the TouchGFX application. This is recommended over using a dummy text. A dummy text will generate all glyphs, but also the actual string (e.g. "0123456789-"). Putting "0123456789-" in this column will generate the glyphs, but not a string.

Widget Wildcard Characters:

These are characters which some widgets that require a wildcard will add. The Digital Clock widget will add "0123456789 :APM" to this field.

/Alexandre

3 replies

Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
July 14, 2021

Hello RReta.1,

You should put your punctuation characters in Wildcard Characters. In general the user does not use Widget Wildcard Characters.

For more information on Text handling, I highly recommend you to check the documentation website

Here is an extract :

Wildcard Characters:

Characters that should be available to display in the TouchGFX application. This is recommended over using a dummy text. A dummy text will generate all glyphs, but also the actual string (e.g. "0123456789-"). Putting "0123456789-" in this column will generate the glyphs, but not a string.

Widget Wildcard Characters:

These are characters which some widgets that require a wildcard will add. The Digital Clock widget will add "0123456789 :APM" to this field.

/Alexandre

RReta.1
RReta.1Author
Associate II
July 14, 2021

Thanks Alexandre! Any ideas on my question on the consumed flash for the glyph in relation to font size? (will the glyph for a larger font size consume more flash?)

Alexandre RENOUX
Visitor II
July 21, 2021

Hello RReta.1,

Yes the flash will be more consumed since it means more information to store ^^

0693W00000D0BJqQAN.png/Alexandre