Skip to main content
Damiano
Associate II
April 13, 2020
Solved

Simulator error with include or extern var

#include <gui/screen1_screen/Screen1View.hpp>
 
#include "../../Core/Inc/hello.h" 			// NO in simulator TouchGFX, Yes in CUBEIDEMX
extern int myvar;							// NO in simulator TouchGFX, Yes in CUBEIDEMX
 
Screen1View::Screen1View()
{
 
}
 
void Screen1View::setupScreen()
{
 Screen1ViewBase::setupScreen();
}
 
void Screen1View::tearDownScreen()
{
 Screen1ViewBase::tearDownScreen();
}
 
void Screen1View::simpleFunc()
{
 ciao();						// err in simulator TouchGFX
 myvar = 7;					// err in simulator TouchGFX
}
#include "hello.h"
 
int myvar = 0;
 
void ciao(void)
{
}
#ifndef APPLICATION_USER_HELLO_H_
#define APPLICATION_USER_HELLO_H_
 
#ifdef __cplusplus
extern "C" {
#endif
 
void ciao(void);
 
#ifdef __cplusplus
}
#endif
 
#endif /* APPLICATION_USER_HELLO_H_ */
#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <touchgfx/Color.hpp>
#include "BitmapDatabase.hpp"
 
Screen1ViewBase::Screen1ViewBase() :
 buttonCallback(this, &Screen1ViewBase::buttonCallbackHandler)
{
 
 box1.setPosition(0, 0, 240, 320);
 box1.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
 
 button1.setXY(35, 130);
 button1.setBitmaps(touchgfx::Bitmap(BITMAP_BLUE_BUTTONS_ROUND_EDGE_SMALL_ID), touchgfx::Bitmap(BITMAP_BLUE_BUTTONS_ROUND_EDGE_SMALL_PRESSED_ID));
 button1.setAction(buttonCallback);
 
 add(box1);
 add(button1);
}
 
void Screen1ViewBase::setupScreen()
{
 
}
 
void Screen1ViewBase::buttonCallbackHandler(const touchgfx::AbstractButton& src)
{
 if (&src == &button1)
 {
 //Interaction1
 //When button1 clicked call virtual function
 //Call simpleFunc
 simpleFunc();
 }
}

Compile in CUBEIDEMX works, run simulator in TOUCHGFX NO

Error in:

#include "../../Core/Inc/hello.h"

or in

extern int myvar;

Thanks

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
April 30, 2020

Hi @Damiano​,

You cannot compile the same code in a simulator project as in CubeIDE. The simulator makefile does not know anything about "Core" because it runs on SDL2. It is usually not best practice to have target specific code in your gui code - If you must, guard it with :

#ifndef SIMULATOR 
/*code*/ 
#endif
 

If you do have code that you need in your simulator you have to manually edit the simulator/gcc/Makefile and update source_paths= and include_paths=

/Martin

3 replies

Alexandre RENOUX
Visitor II
April 14, 2020

Hello,

I do not understand why you have an error because I tried to do the same thing and it worked.

Note: Writing C code in a C++ GUI is not the best way in my opinion. Regarding your goal, you can easily do the same using C++ coding.

I created hello.c in gui\src\common\hello.c and hello.h in gui\include\gui\common\hello.h

Here is the code:

#ifndef APPLICATION_USER_HELLO_H_
#define APPLICATION_USER_HELLO_H_
 
#ifdef __cplusplus
extern "C" {
#endif
 
void ciao(void);
 
#ifdef __cplusplus
}
#endif
 
#endif /* APPLICATION_USER_HELLO_H_ */
#include <gui/common/hello.h>
 
int myvar = 0;
 
void ciao(void)
{
}
#ifndef SCREEN1VIEW_HPP
#define SCREEN1VIEW_HPP
 
#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
 
class Screen1View : public Screen1ViewBase
{
public:
 Screen1View();
 virtual ~Screen1View() {}
 virtual void setupScreen();
 virtual void tearDownScreen();
 
 virtual void simpleFunc();
protected:
};
 
#endif // SCREEN1VIEW_HPP
#include <gui/screen1_screen/Screen1View.hpp>
 
#include <gui/common/hello.h>
extern int myvar;
 
Screen1View::Screen1View()
{
 
}
 
void Screen1View::setupScreen()
{
 Screen1ViewBase::setupScreen();
}
 
void Screen1View::tearDownScreen()
{
 Screen1ViewBase::tearDownScreen();
}
 
void Screen1View::simpleFunc()
{
 ciao();
 myvar = 7;	
}

Damiano
DamianoAuthor
Associate II
April 14, 2020

Hi, thanks for the answer,

my goal is to interface with hardware in TouchGFX applications,

in particular to connect a slider to change the duty cycle of a pwm signal.

The error was here in "run simulator":

 gui/src/screen1_screen/Screen1View.cpp:4:10: fatal error: ../../Core/Inc/hello.h: No such file or directory

     #include "../../Core/Inc/hello.h"

         ^~~~~~~~~~~~~~~~~~~~~~~~

    compilation terminated.

Thanks, with in gui\src\common\hello.c and hello.h in gui\include\gui\common\hello.h

"run simulator" it works.

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
April 30, 2020

Hi @Damiano​,

You cannot compile the same code in a simulator project as in CubeIDE. The simulator makefile does not know anything about "Core" because it runs on SDL2. It is usually not best practice to have target specific code in your gui code - If you must, guard it with :

#ifndef SIMULATOR 
/*code*/ 
#endif
 

If you do have code that you need in your simulator you have to manually edit the simulator/gcc/Makefile and update source_paths= and include_paths=

/Martin