Skip to main content
barms.1
Associate
Jul 24, 2022 5:49 PM UTC
Question

Simulation on Windows 10 error: recipe for target 'generate_assets' failed

I have a fresh install of TouchGFX Designer (4.20.0) running on a Windows 10 computer. Although the code for "Animated Image Example" will generate, the simulation will not compile. I've used all the default settings with no modifications. I'm following this tutorial from TouchGFX.

When running the simulator the log shows:

Run Simulator
 Copy Framework
 Copying TouchGFX framework version 4.20.0 to C:\TouchGFXProjects\MyAnimatedImageExample\touchgfx
 Done
 Generate
 Wrote config/gcc/app.mk
 Wrote config/msvs/Application.props
 Wrote generated/gui_generated/include/gui_generated/common/FrontendApplicationBase.hpp
 Wrote generated/gui_generated/include/gui_generated/common/FrontendHeapBase.hpp
 Wrote generated/gui_generated/include/gui_generated/common/SimConstants.hpp
 Wrote generated/gui_generated/include/gui_generated/main_screen/MainViewBase.hpp
 Wrote generated/gui_generated/src/common/FrontendApplicationBase.cpp
 Wrote generated/gui_generated/src/main_screen/MainViewBase.cpp
 Wrote generated/simulator/gcc/Makefile
 Wrote generated/simulator/include/simulator/mainBase.hpp
 Wrote generated/simulator/include/simulator/video/DirectFrameBufferVideoController.hpp
 Wrote generated/simulator/include/simulator/video/MJPEGDecoder.hpp
 Wrote generated/simulator/include/simulator/video/SoftwareMJPEGDecoder.hpp
 Wrote generated/simulator/msvs/touchgfx_prebuild.targets
 Wrote generated/simulator/msvs/touchgfx_sdl2.props
 Wrote generated/simulator/msvs/touchgfx.props
 Wrote generated/simulator/src/mainBase.cpp
 Wrote generated/simulator/src/video/SoftwareMJPEGDecoder.cpp
 Wrote generated/simulator/touchgfx.ico
 Wrote generated/simulator/touchgfx.rc
 Wrote generated/simulator/touchgfx.res
 Wrote generated/user.config
 Wrote simulator/gcc/Makefile
 Wrote simulator/main.cpp
 Wrote simulator/msvs/Application.sln
 Wrote simulator/msvs/Application.vcxproj
 Wrote simulator/msvs/Application.vcxproj.filters
 Wrote target.config
 Done
 Generate Assets
 make -f simulator/gcc/Makefile assets -j8
 Reading ./application.config
 Generating generated/images/src/image_ani_01.cpp
 Generating generated/images/src/image_ani_02.cpp
 Generating generated/images/src/image_ani_03.cpp
 Generating generated/images/src/image_ani_04.cpp
 Generating generated/images/src/image_ani_05.cpp
 Generating generated/images/src/image_ani_06.cpp
 Generating generated/images/src/image_ani_07.cpp
 Generating generated/images/src/image_ani_08.cpp
 Generating generated/images/src/image_ani_09.cpp
 Generating generated/images/src/image_ani_10.cpp
 Generating generated/images/src/image_ani_11.cpp
 Generating generated/images/src/image_ani_12.cpp
 Generating generated/images/src/image_ani_13.cpp
 Generating generated/images/src/image_ani_14.cpp
 Generating generated/images/src/image_bg.cpp
 Generating generated/videos/include/videos/VideoDatabase.hpp
 Generating generated/images/src/image_btn.cpp
 Generating generated/images/src/image_btn_pressed.cpp
 Generating generated/images/include/BitmapDatabase.hpp
 Generating generated/images/src/BitmapDatabase.cpp
 Cleaning generated files from generated/texts and generated/fonts.
 Generating generated/fonts/include/fonts/GeneratedFont.hpp
 Generating generated/fonts/src/GeneratedFont.cpp
 Generating generated/fonts/include/fonts/UnmappedDataFont.hpp
 Generating generated/fonts/src/UnmappedDataFont.cpp
 Generating generated/fonts/include/fonts/CachedFont.hpp
 Generating generated/fonts/src/CachedFont.cpp
 Generating generated/fonts/include/fonts/FontCache.hpp
 Generating generated/fonts/src/FontCache.cpp
 Generating generated/fonts/src/ApplicationFontProvider.cpp
 Generating generated/fonts/include/fonts/ApplicationFontProvider.hpp
 Generating generated/texts/include/texts/TextKeysAndLanguages.hpp
 Generating generated/texts/include/texts/TypedTextDatabase.hpp
 Generating generated/texts/src/TypedTextDatabase.cpp
 Generating generated/texts/src/Texts.cpp
 Generating generated/texts/src/LanguageGb.cpp
 Done
 Post Generate
 touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
 Done
 Compile
 make -f simulator/gcc/Makefile -j8
 Reading ./application.config
 /usr/bin/sh: -c: line 0: syntax error near unexpected token `('
 /usr/bin/sh: -c: line 0: `C:\Program Files (x86)\GnuWin32\bin\make.exe -f generated/simulator/gcc/Makefile -r -s -rs -j --jobserver-fds=gmake_semaphore_1076 build_executable'
 generated/simulator/gcc/Makefile:155: recipe for target 'generate_assets' failed
 make[1]: *** [generate_assets] Error 258
 simulator/gcc/Makefile:32: recipe for target 'all' failed
 make: *** [all] Error 2
 Failed
 Failed

There is no modification to the Makefile and the result is the same when executing using TouchGFX Environment (4.20.0).

Other similar questions deal with prior versions where the text files are in .xls vs .xml formatting. The only other place I found a reference was to address errors, but that is a different error format than what I've posted. Any thoughts on what is causing this error?

This topic has been closed for replies.

5 replies

Yoann KLEIN
ST Employee
Jul 25, 2022 8:54 AM UTC

Hello @barms.1​ ,

Are you sure that you just followed this tutorial, without doing anything else ?

Because that's the first step of getting started with TouchGFX, and that shouldn't fail in any case.

If yes, can you please share your project, so we can debug it ?

Thanks,

/Yoann

Yoann KLEINST Software Developer | TouchGFX
barms.1
barms.1Author
Associate
Jul 25, 2022 2:48 PM UTC
MyAnimatedImageExample.zip <> Yoann - Here is the project. And I agree, it does seem really odd and it must be something on my end as there is no other reference to anyone having an issue. The only think I could think of is that my gcc/make had some install issue, but from what I can tell TouchGFX runs it's own. Let me know what you think. Thanks, Bill
barms.1
barms.1Author
Associate
Jul 25, 2022 2:48 PM UTC

replied via e-mail given the project size... Thanks.

Yoann KLEIN
ST Employee
Jul 26, 2022 8:14 AM UTC

Hello,

I downloaded your project and ran it directly in the simulator, without any issue.

Could you please try to uninstall and reinstall TouchGFX on your computer, and then start a new project from scratch, like you did previously.

Thanks,

/Yoann

Yoann KLEINST Software Developer | TouchGFX
barms.1
barms.1Author
Associate
Jul 27, 2022 1:10 AM UTC
After uninstalling and reinstalling I get the same compiler error on the demo. But, there are some cached files somewhere that I'd like to delete to make it truly a clean install. After doing the installation it has a pointer to the example project and even the dev board that I had used on the very first instance. I've done a little digging around all the obvious places but cannot find where the 'history' or other cache files are located.
So - still the same error - but not sure I truly got a clean install.