Skip to main content
Visitor II
Jun 30, 2025 1:41 AM UTC
Solved

setVisible() and invalidate() don't work when they are in if/switch~case statement.

emi1123_0-1751247172566.png

I made some containers in 1 screen. (please refer to attached image)

I wanted to handle these containers depends on h/w key.

e.g. temp key is pressed, all of the containers in HDT_POPUP_GRAPHIC_SCREEN must be disabled. only

main_graphic_temp_container will be showed up.

 

However, 

main_graphic_temp_container.setVisible(true);
main_graphic_temp_container.invalidate();

doesn't work normally, when these codes are in the switch~case statement.

emi1123_1-1751247431430.png

 

I tried to move these codes to the end of the setupScreen(), not in the switch~case statement.

In that case, 

main_graphic_temp_container.setVisible(true);
main_graphic_temp_container.invalidate();

works normally.

Am I wrong to use these two (setVisible, invalidate) methods?

 

 

This topic has been closed for replies.
Maxime_MARCHETTOBest answer
ST Employee
Jul 9, 2025 1:37 PM UTC

Hello @emi1123,

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

Best regards,
Maxime

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

GaetanGodart
ST Employee
Jun 30, 2025 9:30 AM UTC

Hello @emi1123 and welcome to the community!

 


Am I wrong to use these two (setVisible, invalidate) methods?


It should be fine.

Can you make sure you do reach that case by adding a print or setting a breakpoint?

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Maxime_MARCHETTOBest answer
ST Employee
Jul 9, 2025 1:37 PM UTC

Hello @emi1123,

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

Best regards,
Maxime

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.