Skip to main content
Associate II
Aug 22, 2023 12:25 PM UTC
Question

Setting up http server on STM32H750B-DK with LwIP and FreeRTOS

Hi,
I am trying to set up an http server on STM32H750B-DK (on STM32CubeIDE) with LwIP. When I program it without implementing FreeRTOS I call the function MX_LWIP_Process in while function in main:

 * Function given to help user to continue LwIP Initialization
 * Up to user to complete or change this function ...
 * Up to user to call this function in main.c in while (1) of main(void)
 *-----------------------------------------------------------------------
 * Read a received packet from the Ethernet buffers
 * Send it to the lwIP stack for handling
 * Handle timeouts if LWIP_TIMERS is set and without RTOS
 * Handle the llink status if LWIP_NETIF_LINK_CALLBACK is set and without RTOS
 */
void MX_LWIP_Process(void)
{
 ethernetif_input(&gnetif);
 sys_check_timeouts();
 Ethernet_Link_Periodic_Handle(&gnetif);
}

The IP address pings fine and the http server is set up. But when I enable FreeRTOS the declaration of this function does not happen:

#if !WITH_RTOS
/* Function defined in lwip.c to:
 * - Read a received packet from the Ethernet buffers
 * - Send it to the lwIP stack for handling
 * - Handle timeouts if NO_SYS_NO_TIMERS not set
 */
void MX_LWIP_Process(void);

#endif /* WITH_RTOS */

Even if I define it outside the if function it doesn’t work. I guess this should work in another way when working with RTOS. I tried calling http_server_init in StartDefaultTask:

static void http_server(struct netconn *conn)
{
	struct netbuf *inbuf;
	err_t recv_err;
	char* buf;
	u16_t buflen;
	struct fs_file file;

	/* Read the data from the port, blocking if nothing yet there */
	recv_err = netconn_recv(conn, &inbuf);

	if (recv_err == ERR_OK)
	{
		if (netconn_err(conn) == ERR_OK)
		{
			/* Get the data pointer and length of the data inside a netbuf */
			netbuf_data(inbuf, (void**)&buf, &buflen);

			/* Check if request to get the index.html */
			if (strncmp((char const *)buf,"GET /index.html",15)==0)
			{
				fs_open(&file, "/index.html");
				netconn_write(conn, (const unsigned char*)(file.data), (size_t)file.len, NETCONN_NOCOPY);
				fs_close(&file);
			}
			else
			{
				/* Load Error page */
				fs_open(&file, "/404.html");
				netconn_write(conn, (const unsigned char*)(file.data), (size_t)file.len, NETCONN_NOCOPY);
				fs_close(&file);
			}
		}
	}
	/* Close the connection (server closes in HTTP) */
	netconn_close(conn);

	/* Delete the buffer (netconn_recv gives us ownership,
 so we have to make sure to deallocate the buffer) */
	netbuf_delete(inbuf);
}


static void http_thread(void *arg)
{ 
 struct netconn *conn, *newconn;
 err_t err, accept_err;
 
 /* Create a new TCP connection handle */
 conn = netconn_new(NETCONN_TCP);
 
 if (conn!= NULL)
 {
 /* Bind to port 80 (HTTP) with default IP address */
 err = netconn_bind(conn, IP_ADDR_ANY, 80);
 
 if (err == ERR_OK)
 {
 /* Put the connection into LISTEN state */
 netconn_listen(conn);
 
 while(1) 
 {
 /* accept any incoming connection */
 accept_err = netconn_accept(conn, &newconn);
 if(accept_err == ERR_OK)
 {
 /* serve connection */
 http_server(newconn);

 /* delete connection */
 netconn_delete(newconn);
 }
 }
 }
 }
}


void http_server_init()
{
 sys_thread_new("http_thread", http_thread, NULL, DEFAULT_THREAD_STACKSIZE, osPriorityNormal);
}

Still doesn’t work. Can anyone help me?

This topic has been closed for replies.

2 replies

Osman SOYKURT
ST Technical Moderator
Aug 24, 2023 9:13 AM UTC

Hello @AK16 ,

I can't help you on this subject as my knowledge concerning it is limited, and your question doesn't seem to be related to TouchGFX. I suggest you move your thread to the Embedded Software (MCU) forum you'll have a better chance of getting an answer.

ST Software Developer | TouchGFX
Pavel A.
Aug 24, 2023 10:59 AM UTC

@AK16 Note that functions in ethernetif.c may be implemented differently with and without RTOS. Make sure that your ethernetif.c follows the right type.