Skip to main content
ssaeb
Associate
April 19, 2020
Question

SDRAM bad resolution on LCD

hello everyone

i have been working with a custom board F429IG

LTDC RGB565

SDRAM 32MB 16bit data width

STMCUBE IDE and CUBEMX 5.6

i have tested each hardware separately and they seem to work fine .

created a project to show just a button in 7" LCD 800X480 resoulotion

at first i programed the micro to use extrenal SDRAM as buffer but the picture went very bad0693W000000W3NbQAK.jpg

then i changed the SDRAM address from 0XC0000000 to internal address of 0X20020000 and i get this result which is perfect

0693W000000W3NgQAK.jpg

here is 2 other pictures from 800x480 test in external memory

0693W000000W3NlQAK.jpg

0693W000000W3NqQAK.jpg

and my memory configuration

 /** Perform the SDRAM1 memory initialization sequence
 */
 hsdram1.Instance = FMC_SDRAM_DEVICE;
 /* hsdram1.Init */
 hsdram1.Init.SDBank = FMC_SDRAM_BANK1;
 hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9;
 hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_13;
 hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16;
 hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
 hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;
 hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
 hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
 hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
 hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;
 /* SdramTiming */
 SdramTiming.LoadToActiveDelay = 2;
 SdramTiming.ExitSelfRefreshDelay = 7;
 SdramTiming.SelfRefreshTime = 6;
 SdramTiming.RowCycleDelay = 6;
 SdramTiming.WriteRecoveryTime = 5;
 SdramTiming.RPDelay = 2;
 SdramTiming.RCDDelay = 2;
 
 if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
 {
 Error_Handler( );
 }
 
 
 HAL_SDRAM_WriteProtection_Disable(&hsdram1);
 HAL_Delay(100);
 FMC_SDRAM_CommandTypeDef command;
 ///////////////////////////////////////////////////////////Clock
 command.CommandMode= FMC_SDRAM_CMD_CLK_ENABLE;
 command.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1;
 command.AutoRefreshNumber=1;
 command.ModeRegisterDefinition=0;
 HAL_SDRAM_SendCommand(&hsdram1, &command, 5000);
 HAL_Delay(10);
 ///////////////////////////////////////////////////////////Precharge
 HAL_Delay(100);
 command.CommandMode= FMC_SDRAM_CMD_PALL;
 command.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1;
 command.AutoRefreshNumber=1;
 command.ModeRegisterDefinition=0;
 HAL_Delay(10);
 ///////////////////////////////////////////////////////////SELF REFRESH
 command.CommandMode= FMC_SDRAM_CMD_SELFREFRESH_MODE;
 command.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1;
 command.AutoRefreshNumber=10;
 command.ModeRegisterDefinition=0;
 HAL_SDRAM_SendCommand(&hsdram1, &command, 5000);
 HAL_Delay(10);
 ///////////////////////////////////////////////////////////MODE SETTINGS
 command.CommandMode= FMC_SDRAM_CMD_LOAD_MODE;
 command.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1;
 command.AutoRefreshNumber=1;
 command.ModeRegisterDefinition=0X00000133;
 HAL_SDRAM_SendCommand(&hsdram1, &command, 5000);
 HAL_Delay(10);
 HAL_SDRAM_SetAutoRefreshNumber(&hsdram1, 730);

My SDRAM is MT48LC16m16

i Think i am missing something but i cant figure it out

i am using no OS and tested the program with and without ChromeART (same result)

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
April 19, 2020

Basic SDRAM test (write some pattern into it and then read it back) without the whole video stuff, works?

JW

ssaeb
ssaebAuthor
Associate
April 19, 2020

yup that was a huge disaster , MODE setting should have been 0x130 , AutoFressh instead of SelfRefresh , and i am now getting the result i wanted took me 5 hours , thanks

HPATH.1
Associate III
November 5, 2020

Hi @ssaeb, can you tell me which memory IC used for 32MB ?