Skip to main content
SMour.2
Associate III
Dec 31, 2020 10:25 AM UTC
Solved

SDMMC Does not work with TouchGFX Application.

Hi,

Iam using a STM32F746 DISCO Board to use SDMMC in a TOUCHGFX Application but Iam not able to get past if(f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(rtext)) != FR_OK) function. It gives error here. Even If I comment this section and reach fopen command it returns FR_DISK_ERR.

However When I simply run the standalone SDMMC example ,it works and writes data to SD card.

Why is that the same example does not work with Touchgfx application?

The only difference I could see is of Clock speed between two applications. One is at 50Hz & other is at 48Hz.

Im Prototyping my project on disco board before I go into custom design. Kindly help!!

This topic has been closed for replies.
SMour.2
SMour.2Best answer
Associate III
Jan 2, 2021 12:26 PM UTC

Hi,

I got it working using FREE RTOS & SDMMC. The mounting of the SD Card needs to be done inside MX_FATFS_Init();

void MX_FATFS_Init(void)

{

 /*## FatFS: Link the SD driver ###########################*/

 retSD = FATFS_LinkDriver(&SD_Driver, SDPath);

 /* USER CODE BEGIN Init */

 /* additional user code for init */

 f_mount(&SDFatFS, (TCHAR const*)SDPath, 0);

 /* USER CODE END Init */

}

It is strange that mounting needs to be done here and not in the RTOS Task.

After Mounting it in the Init function, You can open and write the file inside the RTOS Task like shown below

FRESULT res; /* FatFs function common result code */

uint32_t byteswritten, bytesread; /* File write/read counts */

uint8_t wtext[] = "welcome!"; /* File write buffer */

//uint8_t rtext[_MAX_SS];/* File read buffer */

//f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(rtext));

res = f_open(&SDFile, "test.TXT", FA_CREATE_ALWAYS | FA_WRITE);

res = f_write(&SDFile, wtext, strlen((char *)wtext), (void *)&byteswritten);

f_close(&SDFile);

This is just an example.

I hope it helps others too.

5 replies

MM..1
Super User
Dec 31, 2020 11:52 AM UTC

Try compare your code with GitHub - argandas/STM32F746G-DISCO_TouchGFX_Demo-1: Demo code for STM32F746G-DISCO board using TouchGFX

And where you call  if(f_mkfs((TC ? As you can see on example this need separate thread ... SDTask in demo

SMour.2
SMour.2Author
Associate III
Jan 1, 2021 11:07 AM UTC

Hi,

I created a new task and tried doing the same thing in the new created task . All I did was copied the sdcard example code in another task . But still its not working.

SMour.2
SMour.2AuthorBest answer
Associate III
Jan 2, 2021 12:26 PM UTC

Hi,

I got it working using FREE RTOS & SDMMC. The mounting of the SD Card needs to be done inside MX_FATFS_Init();

void MX_FATFS_Init(void)

{

 /*## FatFS: Link the SD driver ###########################*/

 retSD = FATFS_LinkDriver(&SD_Driver, SDPath);

 /* USER CODE BEGIN Init */

 /* additional user code for init */

 f_mount(&SDFatFS, (TCHAR const*)SDPath, 0);

 /* USER CODE END Init */

}

It is strange that mounting needs to be done here and not in the RTOS Task.

After Mounting it in the Init function, You can open and write the file inside the RTOS Task like shown below

FRESULT res; /* FatFs function common result code */

uint32_t byteswritten, bytesread; /* File write/read counts */

uint8_t wtext[] = "welcome!"; /* File write buffer */

//uint8_t rtext[_MAX_SS];/* File read buffer */

//f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(rtext));

res = f_open(&SDFile, "test.TXT", FA_CREATE_ALWAYS | FA_WRITE);

res = f_write(&SDFile, wtext, strlen((char *)wtext), (void *)&byteswritten);

f_close(&SDFile);

This is just an example.

I hope it helps others too.

Associate II
Mar 11, 2025 9:30 AM UTC

Hi,

I'm still facing the same issue even after following your earlier suggestions.

My code only includes the TouchGFX template and SDMMC functionality. When I debug line by line, it works up to f_mount(), but f_open() fails—even when stepping through the code. If I run the code directly without debugging, f_mount() itself fails.

I suspected a clock issue, so I tried increasing and decreasing the clock speed to verify its impact, but the issue persists. I’m not sure where things are going wrong.
iam using STM32H750XBH6 DEV KIT

 

Associate II
Mar 12, 2025 10:51 AM UTC

From a bit more digging I found that something in the D cache setup seems to have been causing the issue. Adding 'SCB_DisableDCache()' before and 'SCB_EnableDCache()' after any SD card operations seems to solve this issue for me without interfering with TouchGFX in any way. I've only done minimal testing so I cannot guarantee that this solution will work in all situations or be stable long term (I'm not 100% sure what the D-Cache is even used for).

If anyone finds any more information about this, or why disabling the D cache works, I'd be very grateful.