Skip to main content
Msolinas
Senior
Aug 21, 2023 7:13 PM UTC
Question

scrollList HighLight scrolling item

hi all, I need to highlight an item in a scrolllist using two buttons that start scrolling up and down. I managed to implement the routine but I have problems as soon as the system passes into the area of the list that is not yet displayed.

Does anyone have any advice? these are the two code elements that allow the transition with simplicity (even if not 100% functional)

void ProdManagerScreenView::shiftCurrentDrowerUp(void){

 if(selectedDrowerItem>0){

 selectedDrowerItem--;
 HighlItem--;
 scrollList10.animateToItem(selectedDrowerItem,-1);

 clearDrowerSelection();//THIS CLEAR OLD SELECTED
 HilightLineDrowerSelection(0,HighlItem);//HIGHLIGHT NEW ONE

 scrollList10.invalidate();
 //scrollList10.initialize();
 }//

}
//

void ProdManagerScreenView::shiftCurrentDrowerDw(void){

 selectedDrowerItem++;

 if(selectedDrowerItem<scrollList10.getNumberOfItems()){
 HighlItem++;
 //SE SI, ANIMA TUTTO IN PASSI DI 1
 scrollList10.animateToItem(selectedDrowerItem,-1);
 //scrollList10.initialize();

 clearDrowerSelection();//THIS CLEAR OLD SELECTED
 HilightLineDrowerSelection(0,HighlItem);//HIGHLIGHT NEW ONE
 scrollList10.invalidate();
 //scrollList10.initialize();

 } else{
 selectedDrowerItem--;
 }
}
//
 
This topic has been closed for replies.

1 reply

ST Employee
Sep 1, 2023 12:45 PM UTC

Hello @Msolinas ,

I suggest using Scroll Wheel instead of Scroll List because it already has the functionality to focus on one item or in your case, to highlight it. Also, you need to make your Scroll List or Scroll Wheel large enough to accommodate all the elements that you need. It doesn't matter if the list grows out of the screen. 

You can read more about Scroll Wheel here:

https://support.touchgfx.com/docs/development/ui-development/ui-components/containers/scroll-wheel

I hope this will help you

Mohammad MORADIST Software Developer | TouchGFX