Skip to main content
Tuoman
Senior II
Jan 24, 2020 10:48 AM UTC
Question

ScrollList getPositionForItem protected method, cant access

Hello,

Why is this method protected? I want to use this item position to scroll the ScrollList, when cursor is at the bottom (using animateToItem). I use physical buttons to move in the ScrollList.

Must I modify Middleware TouchGFX code to make it public?

Just wondering if this is unelegant solution, is there proper way to do this in TouchGFX, without modifying library code? Thanks!

This topic has been closed for replies.

4 replies

T. Alary
Visitor II
Jan 24, 2020 12:45 PM UTC

Hello,

I want to do exactly the same things ! For the moment, I've managed to do it by calling the drag event handler when the button is pressed.

what is painful is, you have to know from how many pixels you have between each item.

Here's the code used when button is pressed :

scrollList.handleDragEvent( DragEvent(DragEvent::DRAGGED,50,50,100,100));

A method to set scrollList to a specific item would be really appreciated!

Hey Martin!!

Theophile

Martin KJELDSEN
Principal III
Jan 27, 2020 2:06 PM UTC

animateToItem() ?

T. Alary
Visitor II
Jan 28, 2020 10:08 AM UTC

If you have a scrollList with severable item displayed on the screen at the same time, this will not move the liste until the item index correspond to an item that is not viewable. Or have I missed something ?

Tuoman
TuomanAuthor
Senior II
Jan 29, 2020 7:46 AM UTC

Yes. I solve this by scrolling to offset item. E.g. animateToItem() to item+N to get view to item.

P.S. I solved original problem by taking count of items in list, and using that to move the cursor when it goes out of the list range (selecteditem > nrofitems).

Only problem is that i need to manually update count number. Not too bad.