Associate III
July 6, 2021
Question
Screen jitters with animation
- 15 replies
- 3608 views
Hello,
I'm currently developing a project using Touchgfx on a custom board with a STM32F469II, external RAM/FLASH, SD card and a 1024x600 screen.
I've recently come across an issue when performing any animation (slide screen transition, scrollable container, box/circle progress, ...) where the screen shakes like crazy (see video) and also during a small moment after.
Any movement seem to be able to trigger this issue and the only way I've found to stop it is to disable chrom-art but then the frame rate drops down to about 15 fps when performing those animation.
Does anyone know what's causing this shaking ? And if so, how can I limit it as much as possible ?
Thanks in advance,
Tristan