Screen Flickering on Custom HMI with Double Buffer Enabled (STM32H750 + RGB888, 800x480)
- 14 replies
- 1543 views
Hi,
We are encountering a partial screen flickering issue when using a custom HMI with TouchGFX and double buffer enabled. The screen resolution is 800x480, but only the left portion (480x480) displays correctly. The remaining 320x480 area flickers during runtime, especially when updating data on the UI.
Key Observations:
This issue occurs only when double buffering is enabled.
In single buffer mode, minor flickering is still present, but it's significantly better than dual buffer mode.
The issue is isolated to our custom board and BSP configuration.
Cross-Test:
We tested the same TouchGFX button example on two different displays:
Custom Display Board – 800x480 (TFT-LCD, TST070WVBE-31)
→ Flickering observed
Test Board – 1024x600 (other manufacturer)
→ No flickering observed
The main difference:
Custom board: TouchGFX + BSP drivers (manually configured)
Test board: Fully CubeMX-generated configuration
System Configuration:
MCU: STM32H750
Display: TFT-LCD (TST070WVBE-31), 800x480, RGB888
TouchGFX: 4.24.0
STM32CubeIDE: 1.17.0
STM32CubeMX: 6.14.1
Crystal Frequency: 25 MHz
System Clock: 450 MHz
Display Timing Configuration:
Parameter Value
Width (Active) 800
Height (Active) 480
HSYNC 48
HBP 40
HFP 40
VSYNC 1
VBP 31
VFP 13
Horizontal Total = 48 + 40 + 800 + 40 = 928
Vertical Total = 1 + 31 + 480 + 13 = 525
Pixel Clock Calculation:
PLL3M = 5
PLL3N = 40
PLL3R = 6
VCO = (HSE / PLL3M) × PLL3N = (25 MHz / 5) × 40 = 200 MHz
DOTCLK = VCO / PLL3R = 200 MHz / 6 ≈ 33.33 MHz
Frame Rate ≈ 33.33 MHz / (928 × 525) ≈ **68.7 Hz**
Request:
Could anyone suggest what might be causing the flickering on the right side of the screen (320x480) during UI updates with double buffering?
Are there any known limitations with partial redraws or framebuffer alignment for RGB888 mode?
Could manual invalidateRect() or framebuffer region management be affecting this?
Any experience comparing CubeMX vs. custom BSP configurations in such cases?
We’ve attached the relevant configuration files and video evidence for reference.
Please let me know if additional details are required. Any insights or suggestions to help resolve this issue would be greatly appreciated!
Best regards,
Shekhar