Skip to main content
Senior
Apr 24, 2025 7:06 AM UTC
Solved

Screen code not generated by TouchGFX unless the screen is used/called?

Hi,

it seems that unless I make some transition to a specific screen within touchGFX (i.e. a button changing another screen to the screen in question), then TouchGFX does not generate any code for that screen (view, presenter, etc).

I guess it makes sense in order to save memory. But I want to transition to that screen programmatically so I do need all the code to be generated for that screen.

Is there some other way to force TouchGFX to generate the code for that screen?

Thank you

Ricko_0-1745477897243.png

 

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
Apr 24, 2025 9:30 AM UTC

Hello @Ricko ,

 

You could create an interaction where the trigger will never happen and the action is to switch to screen X, this way you get your code generated.

One way to add a trigger that will never be called is to select the "hardware button clicked" (as long as you don't use a physical keyboard in your final project):

GaetanGodart_0-1745486923498.png

Alternatively, you could create an action on the screen and use that action as a trigger (this action will never be called if you don't do that yourself) :

GaetanGodart_1-1745486966458.png

 

Regards,

 

Gaetan GodartSoftware engineer at ST (TouchGFX)

3 replies

GaetanGodart
GaetanGodartBest answer
ST Employee
Apr 24, 2025 9:30 AM UTC

Hello @Ricko ,

 

You could create an interaction where the trigger will never happen and the action is to switch to screen X, this way you get your code generated.

One way to add a trigger that will never be called is to select the "hardware button clicked" (as long as you don't use a physical keyboard in your final project):

GaetanGodart_0-1745486923498.png

Alternatively, you could create an action on the screen and use that action as a trigger (this action will never be called if you don't do that yourself) :

GaetanGodart_1-1745486966458.png

 

Regards,

 

Gaetan GodartSoftware engineer at ST (TouchGFX)
RickoAuthor
Senior
Apr 25, 2025 3:07 AM UTC

Thank you again @GaetanGodart  :)

GaetanGodart
ST Employee
Apr 25, 2025 7:51 AM UTC

My pleasure! :)

Gaetan GodartSoftware engineer at ST (TouchGFX)