Skip to main content
Jul 9, 2020 5:42 PM UTC
Question

Sample code for stm32f429 and Touchgfx with Keil

Hello All,

I have tried using stm32cube for making a basic project with stm32f429(igt6) series and Touchgfx for keil.

1) I wonder if touchgfx itself does the initialization of LCD or not? If not where should I add that?

2) How can I configure Ram? FMC for nand flash and RAM has been enabled in advance (not completeley configured).

3) Is there any working sample code available for these series?

This topic has been closed for replies.

11 replies

Alexandre RENOUX
Visitor II
Jul 15, 2020 11:56 AM UTC

Hello,

Please have a look at the documentation https://support.touchgfx.com/docs/development/touchgfx-hal-development/touchgfx-generator

Also, you will find the F429-DISCO and EVAL board Application Template available in TouchGFX Designer.

/Alexandre

Vdoij.1
Associate II
Aug 21, 2023 1:35 PM UTC

Page not found

Jul 16, 2020 6:43 AM UTC

Sorry but yours answer does'nt really solve the problem.

Some other engineer really helped me and all maters had solved. Maybe I will publish some video. There are some wonderful working tutorial in Persian.

MNapi
Senior II
Jul 16, 2020 12:07 PM UTC

I am having myself problem to to start a project with LCD. touchgfx itself does the initialization of LCD but when you open project from the MDK-ARM folder in Keil it will not compile, it throws bunch of errors.

I do not see that touchgfx would allow you to draw customs graphics. Which is a serious setback if you need to display incoming data.

The best option I see now is to use the drivers they have in this file en.stm32cubef4_v1-25-0 you download they are called BSP drivers. There are also a few examples which work in Keil (using those drivers) you can modify to your own use.

They did good boards but thye do not give you good video tutorial to learn it, you have to learn from other people on YouTube. This is why Ardunio is so popular becasue you can find all the code you need.

Jul 16, 2020 1:09 PM UTC

To tell the truth, I have been able to run Touchgfx on STM32F429IGT6 with the support of external RAM. As I said there is a complete tutorial in Persian. In case the tutor allow me, I will translate the video and publish it.

BWeal.1
Visitor II
Jan 6, 2021 12:46 AM UTC

go in the market and found any library about fixed this issue I don't think so you will get any kind of information online because I had also face this issue and fixed the problem by an expert.

purenetworth