RTC update lag
Hello dear friends,
The problem I have encountered is that updating the digital clock takes too much time. So I can see that some time updating takes up to 3 seconds, it is wonderful that other widgets don't stop and do their work.
I didn't understand what is really the source of the problem.
I use HAL for reading RTC, using the digital clock widget.
Touchgfx version: 4.15 (Didn't dare to upgrade to 4.16)
RTOS: Not yet used. (Planed for next times)
UC: STM32f429IGT6
USB: CDC Enabled
Compiler: Keil V5.32
Any help would be appreciated.