Skip to main content
cb.7
Associate III
Feb 6, 2025 10:21 AM UTC
Question

Rotate screen 180 degrees

I would like to rotate my screen 180 degrees, I know that Touchgfx does not support this option but it is possible to do so by modifying the internal registers of the display controller.
In my case the display has a resolution of 480x272 and the controller is an HX8247-A and I only have the RGB interface available, I do not have access to the pins for screen rotation but I saw that I have to set the UD and LR bits of the 'Driver Data Control' register to a low level.
Do you think it is possible to modify the internal registers via the LTDC peripheral of the microcontroller (STM32H7)?
Thanks

This topic has been closed for replies.

2 replies

mƎALLEm
ST Technical Moderator
Feb 6, 2025 11:29 AM UTC
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
cb.7
cb.7Author
Associate III
Feb 6, 2025 2:16 PM UTC

I had already seen these old posts but I was wondering if it was possible to access the HX8247-A controller registers via RGB interface. Unfortunately I do not have access to the controller SPI pins....