Skip to main content
Associate II
Jun 25, 2025 12:26 PM UTC
Question

Reuse assets without creating a copy

Hello

I have a lot of assets, both images and texts, that I need to use across multiple projects. Is it possible to link to the assets without creating a local copy in the project?

When I add an image in the designer it copies from the original location to the project assets\images folder. Can I not just set a relative link from the project folder to the folder that holds the assets?

 

Thank you in advance.

This topic has been closed for replies.

4 replies

mƎALLEm
ST Technical Moderator
Jun 25, 2025 12:49 PM UTC

Hello @Aagaard and welcome to the ST community,

In the TouchGFX designer, simply browse to the folder where the images are located in your local disc:

1- Select the image option

2- Click on "Project"

3- Click on "+" behind "images". You will prompted to the explorer.

mALLEm_0-1750855610572.png

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
AagaardAuthor
Associate II
Jun 25, 2025 12:54 PM UTC

I know how to add images to the project. This creates a local copy, just like going into images and importing.
I want to add a path to the image without generating the local copy.

Ozone
Principal
Jun 25, 2025 12:55 PM UTC

If I remember correctly, there are general Eclipse methods to achieve such shared ("linked") resources.

Although this has always been one of the most awkward and anti-intuitive topics with Eclipse ...

ST Employee
Jun 25, 2025 1:06 PM UTC

Hello @Aagaard,

There's no way to do it out of the box, you can also do some versioning git.

 

Br, 

Louis BOUDOST Software Engineer | TouchGFX