Skip to main content
Anders Nedergaard PETERSEN
Senior II
Nov 27, 2018 9:47 AM UTC
Question

REPOST: scrolling ScrollableContainer

QUESTION - TouchGFX Community repost - Tomasz Lasota - Sep 2017

Hello

How to scroll programatically to a cretain entry in the list?

ScrollableContainer::doScroll() - is protected

Tomasz

ANSWER - TouchGFX Community repost - Martin Kjeldsen - Sep 2017

You could create a MyScrollableContainer as a subclass of ScrollableContainer. Then you can make a public function myScroll() which calls the protected ScrollableContainer::doScroll() function.

ANSWER - TouchGFX Community repost - Tomasz Lasota - Sep 2017

I did

#include <touchgfx/containers/ScrollableContainer.hpp>

using namespace touchgfx;

class MyScrollableContainerA :

public ScrollableContainer

{

public:

MyScrollableContainerA();

~MyScrollableContainerA();

bool doScroll(int16_t deltaX, int16_t deltaY);

};

#include "MyScrollableContainerA.h"

MyScrollableContainerA::MyScrollableContainerA()

{

}

MyScrollableContainerA::~MyScrollableContainerA()

{

}

bool MyScrollableContainerA::doScroll(int16_t deltaX, int16_t deltaY)

{

return doScroll(deltaX, deltaY);

}

call function

scrollableMenu.doScroll(0, 0);

or 

scrollableMenu.doScroll(0, 1);

and I have in doScroll

Unhandled exception at 0x00CA5169 in Application.exe: 0xC0000005: Access violation writing location 0x00860F34.

--

I was wrong

bool MyScrollableContainerA::doScroll(int16_t deltaX, int16_t deltaY)

{

return ScrollableContainer::doScroll(deltaX, deltaY);

}

thank you 

works correctly

This topic has been closed for replies.