Skip to main content
KNara.2
Associate III
Nov 7, 2024 9:19 AM UTC
Question

Repeated images in animation

Hi All,

Is there a way to avoid repeated images in animation?

To be more specific lets say I have animation to be created with 6 .png images and lets say my first 2 images and last 2 images are  the same...Is there a way to reuse the same images (1.png and 2.png ) instead of repeating the copy of the images ?
As of now I'm simply naming the images as 1.png 2.png 3.png 4.png 5.png(copy of 2.png) and 6.png(copy of 1.png).

 

Can I eliminate the 5 and 6 and reuse 1 and 2?
How can I make it more efficient?

 

Thanks & Regards,

This topic has been closed for replies.

3 replies

MM..1
Super User
Nov 7, 2024 1:34 PM UTC

Why not, create animation in your user code ... Animated Image | TouchGFX Documentation

 

animatedImage.setBitmaps(BITMAP_BUTTERFLY_01_ID, BITMAP_BUTTERFLY_72_ID);

 

 

then seems must be manipulated IDs database manualy... Designer dont have inteligent solution for this.

GaetanGodart
ST Employee
Nov 8, 2024 9:13 AM UTC

Hello @KNara.2 ,

 

There is no inherent way to do that.

However, you could simple go into the code and loop back the animation with the methods we provide or do almost anything for that matter.
Alternatively, if I had to do that myself, I would add 2 animated images, one for the animation from image 1 to image 4 and one from image to image 1, the start of the second animated image is triggered by the end if the first animated image, this allows you to have your expected behavior without having copies of your images, in that case you simple reuse the same image but in another animated image.

 

If one of the comments helped you, I invite you to select it as "best answer". :smiling_face_with_smiling_eyes:

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
GaetanGodart
ST Employee
Nov 25, 2024 2:32 PM UTC

Hello @KNara.2 ,

 

Have you been able to move forward on your issue?

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)