Skip to main content
lchac.1
Visitor II
Mar 15, 2023 6:22 AM UTC
Question

region `FLASH' overflowed by 850456 bytes , This is the error I am getting while compiling the files , I Just try to add an image of size 140 kb then it is showing the error, after removing the image still I get the same error , can anyone explain th

..

This topic has been closed for replies.

2 replies

Osman SOYKURT
ST Technical Moderator
Mar 15, 2023 8:24 PM UTC

Hello lchac.1,

Could you tell us a bit about your configuration? Is your project based on a TBS (TouchGFX board setup) or is it a custom board? Whis version of TouchGFX do you use? Which compiler do use?

To me it looks like an issue related to your memory mapping. How did you define your memory regions in your linker script?

/Osman

ST Software Developer | TouchGFX
Tesla DeLorean
Guru
Mar 15, 2023 9:04 PM UTC

>> can anyone explain this

Based on your presentation of the facts, no.

The question doesn't have to fit entirely into the Title/Summary, use the body of the question, you can edit posts, and provide more detail, attach images or files.

If this just happened, I'd supposed you added multiple instances of the file.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..