Skip to main content
NHo.1
Associate III
May 23, 2020
Question

Reduce RAM for UI

Hi ST,

How to reduce RAM for Screen.

Ex: I defines 3 buttons into custom container and add this custom container into screens. I just want to show 1 button in once screen. How to reduce RAM for 2 buttons not use of custom container?

Please help, thanks!

This topic has been closed for replies.

1 reply

Alexandre RENOUX
Visitor II
May 25, 2020

Hello,

If you don't want to show 3 buttons on each screen, do not add 3 buttons to a custom container that you will add to each screen. Why do you want to use a Custom Container ? If you want to show one button in one screen, then add only one button to this screen. Please provide more information.

To reduce RAM you can lower the color depth. For example going to RGB888 to RGB565 or even to L8 if you only use a few sets of color for your assets (https://support.touchgfx.com/docs/development/ui-development/scenarios/using-the-l8-image-format-to-reduce-memory-consumption)

Some info regarding color formats : https://support.touchgfx.com/docs/basic-concepts/color-formats

/Alexandre