Skip to main content
Associate II
Feb 14, 2025 3:55 PM UTC
Question

qspi with touchgfx in stm32f469i dico board

hello everyone..

i am getting problem in the stm32f469 disco board while using the QSPI along with the touchgfx, i worked previously only on Qspi with external loader what ever stm given and it worked fine but after that i configured project from tochgfx the IDE, IDE it self Enable and give the configuration some other peripheral, i am using qspi with default configuration  whatever by touchgfx IDE given itself, i am not able to write and read to External QSPI flash even though i am following same procedure what ever i followed while working without touchgfx. if i disable memory mapped mode it is going to error handler.

please some one suggest solution why the QSPI is not  working with touchgfx.

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
Mar 4, 2025 1:40 PM UTC

Hello @Abhishek_nr,

 

Which 32F469IDISCOVERY board revision are you using?

I recommend you to test the TouchGFX demonstration under \STM32Cube\Repository\STM32Cube_FW_F4_V1.28.1\Projects\STM32469I Discovery\Demonstrations\TouchGFX. Then, try to test the demo using STM32CubeProgrammer. For that, please flash the touchGFX demo.hex with MT25QL128A_STM32F469I-DK NOR_flash External loaders.

KDJEM1_0-1741095597650.png

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.